Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Low wattage 110v over 20-22AWG wire?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 13 replies
  • Subscribers 507 subscribers
  • Views 5112 views
  • Users 0 members are here
  • wiring
  • nodemcu
Related

Low wattage 110v over 20-22AWG wire?

DanTheMan827
DanTheMan827 over 9 years ago

I bought a 5v power supply from china but the holes in the PCB for the AC voltage are extremely small (about 20-22AWG)

 

Is this safe to use with such a thin wire?

 

I mean, my measurements are just a guess but I did try some 18AWG stranded wire and it didn't fit through the hole... (almost)

 

Here's a spec sheet for the PSU http://shop.cpu.com.tw/product/48432/info/

 

I plan on stuffing a NodeMCU, relay, and this power supply into a single gang blue electrical box that will not be mounted inside the wall but instead would be something like an all-in-one powerswitch tail.

 

I plan to use as a Wi-Fi light switch for patio lighting (a series of 12V LED lights) which would be used in place of an existing wall-mounted timer.

 

I was thinking of wiring it up something like this, the 110VAC coming in would be a recycled PC power cord.

 

FlaUmey.png

 

Since it will be inside a electrical box the branch of 110V to the 5v psu would be very short.

 

I would use a wire nut for the neutral wires which would be the light wire, PSU neutral, and the neutral from the outlet

 

Then for the hot it would be the same but the light wire would be passing through the relay instead.

 

Also, would I safely be able to remove some strands of from a thicker wire to fit it through the PCB hole?

  • Sign in to reply
  • Cancel

Top Replies

  • gdstew
    gdstew over 9 years ago +1
    As long as the wire insulation is rated above the AC voltage (usually 300V) and the current used by the LED strip is below what 20 - 22 gauge wire is rated for which is 5A (22 ga.) - 6A (20 ga.) for solid…
  • jw0752
    jw0752 over 9 years ago in reply to Jan Cumps +1
    I was just looking for reinforcements for the next time D_Hersey decides to invade Wisconsin with his profound rhetoric. Also Wausau is a really great place with lots to see. I used to go there once a…
Parents
  • the-dubster
    0 the-dubster over 9 years ago

    Unless I'm being a bit daft, the request is about the Input current. No spect for the input draw but here is some comparisons.

     

    I have a few 240V in 5V out wall warts lying around, Specs are:

     

    Apple iPad     - Input 100-240V AC @ 0.45A (so 450mA)

                          - Output 5.1V DC - 2.1A

     

    Huawei          - Input 100-240V AC @ 0.2A (so 200mA)

                          - Output 5V DC - 1A

     

    Apple iPhone - Input 100-240V AC @ 0.15A (so 150mA)

                          - Output 5V DC - 1A

     

    22awg has a rating of about 7A, so yeah, ensure it's mains rated for insulation and you SHOULD be ok!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • DanTheMan827
    0 DanTheMan827 over 9 years ago in reply to the-dubster

    I actually did find a spec sheet after posting the question, http://shop.cpu.com.tw/product/48432/info/

     

    From what I can gather it uses 0.0273A under full load conditions with a 20A surge/inrush current..

     

    I have some stranded 18AWG wire from a broken 3-speed ceiling fan switch

     

    Could I remove some of the copper wire strands after/during stripping to make it 20AWG?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • DanTheMan827
    0 DanTheMan827 over 9 years ago in reply to the-dubster

    I actually did find a spec sheet after posting the question, http://shop.cpu.com.tw/product/48432/info/

     

    From what I can gather it uses 0.0273A under full load conditions with a 20A surge/inrush current..

     

    I have some stranded 18AWG wire from a broken 3-speed ceiling fan switch

     

    Could I remove some of the copper wire strands after/during stripping to make it 20AWG?