Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Standardisation?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 17 replies
  • Answers 8 answers
  • Subscribers 504 subscribers
  • Views 2503 views
  • Users 0 members are here
Related

Standardisation?

Workshopshed
Workshopshed over 9 years ago

Following on from a discussion about the Intel Edison being discontinued I got thinking about what could be used as a replacement for longer lifetime projects. The Pi compute module was mentioned but that form factor is a single supplier again. I understand you can get suppliers to sign up to longer term support but that's no good unless you are one of the big companies.

 

So I was wondering if there were any small form factor standards for processor boards that would allow you to have multiple supplier options?

 

I spotted Smarc 2.0 which has a option for 82 mm × 50 mm boards https://www.sget.org/standards/smarc.html

and

96Boards IOT (which only has 2 boards and one supplier at the moment) - 96Boards - Internet of Things Edition

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 9 years ago +3 suggested
    Hi Andy! Really good topic. I think there was such a discussion a few years ago, but time has moved on and this topic is worthwhile examining from fresh with current information. From my perspective, I…
  • DAB
    DAB over 9 years ago +3 suggested
    Hi Andy, Interesting post. Board size is usually determined by the functions implemented. I think that was the key reason for the Arduino, TI, BeagleBone, and RPi support boards. Each vender determines…
  • Workshopshed
    Workshopshed over 9 years ago in reply to shabaz +2 suggested
    >I feel the availability for the parts and ease-of-use for using the parts and associated software is more important than the pin compatibility I was thinking a bit more than just the pinout, the form…
Parents
  • shabaz
    0 shabaz over 9 years ago

    Hi Andy!

     

    Really good topic. I think there was such a discussion a few years ago, but time has moved on and this topic is worthwhile examining from fresh with current information.

    From my perspective, I feel the availability for the parts and ease-of-use for using the parts and associated software is more important than the pin compatibility, but I can appreciate that for many projects the two go hand-in-hand.

     

    In terms of availability, the BeagleBone modules (i.e. AM335x TI Sitara) are highly desirable because TI has discussed a typical 10-year product life on Sitara devices. Also, for form-factor, it offers a lot of flexibility because even if people don't want to work with the processor directly, they can pick up a module, such as the OSD335x which integrates the processor, DRAM and other stuff. It isn't quite as integrated as Edison sadly : (

    The module is usable even by hobbyists, so is just as easy to use as Edison. Also companies like Olimex have modules based on the same chipset. And the BeagleBoard project means there is no need to build and maintain an image, Ubuntu for it already exists.

    So, for me, it seems like BeagleBone design is still the way forward for now, since even if a form-factor board disappears, it would not be hard to create your own using the OSD335x.

     

    I've thought a lot about it in recent times and in terms of connectors, if I had to design a board, I don't really like the DIMM slot design, and my ideal board would have a combination of some (very few) 0.1" pins (for I2C, SPI and a few I/O), but also a higher density low profile connector with all the rest of the connections. For that, the Edison style connector was very good, it was dense but still manageable for hobbyist use too. And the board would be tiny, it should be smaller than credit-card size. In other words, almost like Edison : )

     

    Anyway, that is just some thoughts, others will have perhaps totally different ideas about their preferred modules/form-factors etc.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 9 years ago

    Hi Andy!

     

    Really good topic. I think there was such a discussion a few years ago, but time has moved on and this topic is worthwhile examining from fresh with current information.

    From my perspective, I feel the availability for the parts and ease-of-use for using the parts and associated software is more important than the pin compatibility, but I can appreciate that for many projects the two go hand-in-hand.

     

    In terms of availability, the BeagleBone modules (i.e. AM335x TI Sitara) are highly desirable because TI has discussed a typical 10-year product life on Sitara devices. Also, for form-factor, it offers a lot of flexibility because even if people don't want to work with the processor directly, they can pick up a module, such as the OSD335x which integrates the processor, DRAM and other stuff. It isn't quite as integrated as Edison sadly : (

    The module is usable even by hobbyists, so is just as easy to use as Edison. Also companies like Olimex have modules based on the same chipset. And the BeagleBoard project means there is no need to build and maintain an image, Ubuntu for it already exists.

    So, for me, it seems like BeagleBone design is still the way forward for now, since even if a form-factor board disappears, it would not be hard to create your own using the OSD335x.

     

    I've thought a lot about it in recent times and in terms of connectors, if I had to design a board, I don't really like the DIMM slot design, and my ideal board would have a combination of some (very few) 0.1" pins (for I2C, SPI and a few I/O), but also a higher density low profile connector with all the rest of the connections. For that, the Edison style connector was very good, it was dense but still manageable for hobbyist use too. And the board would be tiny, it should be smaller than credit-card size. In other words, almost like Edison : )

     

    Anyway, that is just some thoughts, others will have perhaps totally different ideas about their preferred modules/form-factors etc.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • Workshopshed
    0 Workshopshed over 9 years ago in reply to shabaz

    >I feel the availability for the parts and ease-of-use for using the parts and associated software is more important than the pin compatibility

    I was thinking a bit more than just the pinout, the form factor, power requirements, aerial placement and software (I forgot to mention that) are all important. I'd agree that for some things the tool chain is important but for a Linux based board how much of an issues is that?

     

    >In terms of availability, the BeagleBone modules (i.e. AM335x TI Sitara) are highly desirable

    I totally agree that if a supplier has agreed a 10 year life (and we are not already on year 9) then that would be a good choice.

     

    >And the board would be tiny, it should be smaller than credit-card size.

    I typically prefer a small board over a powerful board

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Workshopshed
    0 Workshopshed over 9 years ago in reply to shabaz

    The Pocketbone has potential, although I/O is a bit sparce

     

    https://hackaday.io/project/19495-pocketbone-kicad

     

    Hand Assembly of pocketbone

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer