Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum What is a modern substitute for venerable EPROMs?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 5 answers
  • Subscribers 504 subscribers
  • Views 3188 views
  • Users 0 members are here
  • non volatile memory
  • microprocessor
  • eprom
  • embedded
Related

What is a modern substitute for venerable EPROMs?

SGarciaV
SGarciaV over 9 years ago

Hi all,

 

I am doing some preliminary research for a possible project for next year. The project, in general terms, involves an embedded system with a uProcessor and external nonvolatile memory for firmware.

 

Over 20 years ago I worked with EPROMs; however, since we are now in the "Jetson" era, I wondered if there was a modern replacement for the EPROM.

 

I am aware of flash-able EEPROMs that can be programmed in circuit via software. I have flashed the BIOS on PCs using this technique. Also, this type of technology is at the core of the SSD, whether it is a 250GB device or a smaller 32GB USB thumb drive.

 

What sort of memory component can I use instead of the EPROM? Capacity can range from 8K to 32K. The device does not have to be pin compatible with the EPROMs. but should have similar functionality and be able to interface with either 3.3 or 5v devices (I am tending towards 5v).

 

Thank you for your time and assistance. Sgarciav

  • Sign in to reply
  • Cancel

Top Replies

  • rachaelp
    rachaelp over 9 years ago +4 suggested
    Hello, How about FRAM? Something like this: http://www.cypress.com/file/41731/download Best Regards, Rachael
  • jc2048
    jc2048 over 9 years ago +3 suggested
    You can still get parallel EEPROMS. This one is 32Kx8, 5V supply, and with 150nS access. Very similar to an EPROM. http://www.microchip.com/wwwproducts/en/AT28C256 Have a look around their memory section…
  • pettitda
    pettitda over 9 years ago +2 suggested
    For storing firmware, flash memory is pretty much the modern equivalent of the EPROM. Most micro controllers include on-board flash memory of at least 32k up to 1M or more.
  • jc2048
    0 jc2048 over 9 years ago

    You can still get parallel EEPROMS. This one is 32Kx8, 5V supply, and with 150nS access. Very similar to an EPROM.

     

    http://www.microchip.com/wwwproducts/en/AT28C256

     

    Have a look around their memory section to see what else they've got.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • rachaelp
    0 rachaelp over 9 years ago

    Hello,

     

    How about FRAM? Something like this: http://www.cypress.com/file/41731/download

     

    Best Regards,


    Rachael

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • pettitda
    0 pettitda over 9 years ago

    For storing firmware, flash memory is pretty much the modern equivalent of the EPROM.  Most micro controllers include on-board flash memory of at least 32k up to 1M or more. 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • SGarciaV
    0 SGarciaV over 9 years ago in reply to jc2048

    Ok, thanks. I will look into this. This is exactly what I am looking for, but... that FRAM recommendation looks awfully tempting. :-)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • SGarciaV
    0 SGarciaV over 9 years ago in reply to rachaelp

    I was thinking more EEPROM, but I admit that I had not considered this option. Looking at some preliminary information, I see that these components have an SPI interface, so it might be feasible to build a programmer.

     

    While EEPROM was more on my mind, it seems that building a programmer might be more complicated.

     

    Truth be told, I ca test both technologies and see which one I like best,

     

    Thanks for the input!

     

    PS: I think that the correct answer is both FRAM and EEPROM, but I can only mark one post as "correct" bummer!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • SGarciaV
    0 SGarciaV over 9 years ago in reply to pettitda

    Thanks David!

     

    For this particular project I am moving away from microcontrollers, hence the quest for an external nonvolatile memory component. However, I do have Yet Another Project that is shelved at the moment that will be using a microcontroller and I will be needing at least 64KB non volatile memory (internal to the uC). Could you reference a specific line or family of uControllers that have this internal flash memory? Thanks! Sgarciav

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 9 years ago in reply to SGarciaV

    Salvador Garcia wrote:

     

    I do have Yet Another Project that is shelved at the moment that will be using a microcontroller and I will be needing at least 64KB non volatile memory (internal to the uC). Could you reference a specific line or family of uControllers that have this internal flash memory? Thanks! Sgarciav

    I like the STM32 parts from STMicroelectronics.  They have a broad line of ARM Cortex parts with a wide range of price, performance, and power consumption.  I've been programming the STM32F103C8 MCU which STM32 Discovery boards use as their ST-Link programming/debug processor.  It has ARM Cortex-M3, 64KB Flash, 20KB SRAM, and a full-speed USB device interface along with the usual GPIOs, SPI, UARTs, etc.  Very nice MCU.  Good documentation, except for the USB section which badly needs rewriting.

     

    I've never used ST's software -- I've done all development using FLOSS (Free-as-in-Liberty Open Source Software) tools over SWD ("Single Wire" Debug).  So far, ST and ARM documentation have been complete enough to allow this.

     

    There are other MCU vendors with similar capabilities.  I'll let their fans make their own comments.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • pettitda
    0 pettitda over 9 years ago in reply to SGarciaV

    I have personal experience with the Texas Instruments MSP430 line of micro controllers.  They have a wide range of parts with varying peripheral sets, amounts of internal flash, and amounts of internal SRAM.  However, there are many other vendors and product families that have internal flash.  It just depends are what your requirements are.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dougw
    0 dougw over 9 years ago in reply to pettitda

    The TI MSP430FR5x and MSP430FR6x MCUs have up to 128KB of internal FRAM.

    CY8CKIT-044 PSoCRegistered 4 M-Series Pioneer Kit has 1Mbit of FRAM.