Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Boost a 0-10mV input signal to Microcontroller (STM32) ADC
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 3 answers
  • Subscribers 503 subscribers
  • Views 2156 views
  • Users 0 members are here
Related

Boost a 0-10mV input signal to Microcontroller (STM32) ADC

iamdevise
iamdevise over 7 years ago

Hello,

I have a Load cell which generates an output of 0-10 mV. I have to read this output of the Load Cell into my micro-controller (using the in-built ADC peripheral). My controller is a STM32F4 family controller which works off a 3.3 V supply.

I have researched possible options of:

  • Using an Op-Amp, adjust gain and feed output to Controller ADC.
  • Use an Instrumentation Amplifier, adjust gain and feed output to Controller ADC.
  • Use an external ADC which works in the 0-10 mV range and feed output to Controller ADC.

 

I am more Firmware developer and not very familiar with which technique would work and which won't. Any suggestions? If none of the above, do let me know which area to research so that I can delve into that as well.

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 7 years ago +5 suggested
    You could check my blogs about a solution I designed to handle a compression load cell to see if it works for you: Sixth Sense - Sensor Circuits - GraffitiBot blog 3 Sixth Sense - Load Cell PCB - GraffitiBot…
  • michaelkellett
    michaelkellett over 7 years ago +3 suggested
    Lots of additional questions need answers before I can give more than a very general response. Like: Will the load cell output always be positive - load cells have offsets so the output with zero load…
  • rsc
    rsc over 7 years ago +2 suggested
    I would suggest a two-stage amplifier using low-noise differential pair inputs and shielded twisted pair cables from the load cell. You can easily get a few mV of electrical noise in a room just from light…
Parents
  • rsc
    0 rsc over 7 years ago

    I would suggest a two-stage amplifier using low-noise differential pair inputs and shielded twisted pair cables from the load cell.

    You can easily get a few mV of electrical noise in a room just from light fixtures. Power from a battery will also reduce noise.

    Scott

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • rsc
    0 rsc over 7 years ago

    I would suggest a two-stage amplifier using low-noise differential pair inputs and shielded twisted pair cables from the load cell.

    You can easily get a few mV of electrical noise in a room just from light fixtures. Power from a battery will also reduce noise.

    Scott

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer