Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum reproducing sine wave accurately
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 4 answers
  • Subscribers 502 subscribers
  • Views 1377 views
  • Users 0 members are here
  • cortex-m0 mcu
Related

reproducing sine wave accurately

gnsh
gnsh over 6 years ago

I am using a cortex M0 microcontroller. i am giving a  sine wave input of 1 Hz. this input signal is given to a 12 bit adc and this converted data is given to uart This uart data Im plotting through a serial plotter. image

 

 

how to get a smooth sine wave? from the uart data.

Attachments:
SINEWAVE.c.zip
  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 6 years ago +4 suggested
    So many things could be wrong that it's hard to know where to start suggesting. What does you code do, and where did it come from. How fast are you sampling, how is the data being presented to the UART…
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to michaelkellett +3 suggested
    I found this function in the attachment: int32_t adc_sine(void) { int32_t u32Result; unsigned char buffer[20]; ADC_Open(ADC, ADC_INPUT_MODE_SINGLE_END, ADC_OPERATION_MODE_CONTINUOUS, ADC_CH_1_MASK);…
  • shabaz
    shabaz over 6 years ago in reply to Jan Cumps +3
    He's using sprintf with %d, so not sending the number, but an ASCII representation. I don't know what his serial plotter is doing, but maybe it is mashing up the characters into nonsense words or long…
Parents
  • michaelkellett
    0 michaelkellett over 6 years ago

    So many things could be wrong that it's hard to know where to start suggesting.

     

    What does you code do, and where did it come from.

     

    How fast are you sampling, how is the data being presented to the UART (binary, text ???)

     

    What hardware and programming/debugging tools are you using.

     

    The amplitude of the samples may be a clue: The 12 bit ADC will give readings from 0 - 4097, but your plot is showing data in the range 7.5E8 to 9.5E8 - that's not right.

     

    MK

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 6 years ago in reply to michaelkellett

    I found this function in the attachment:

     

    int32_t  adc_sine(void)
    {
    int32_t u32Result;
    unsigned char buffer[20];
    
      ADC_Open(ADC, ADC_INPUT_MODE_SINGLE_END, ADC_OPERATION_MODE_CONTINUOUS, ADC_CH_1_MASK);
    
    
        // Set reference voltage to AVDD
        ADC_SET_REF_VOLTAGE(ADC,ADC_REFSEL_INT_VREF);
    //    // Power on ADC
        ADC_POWER_ON(ADC);
    
    
        ADC_START_CONV(ADC);
    
    
       // while (u8ADF == 0);
    
    
        u32Result = ADC_GET_CONVERSION_DATA(ADC, 1);
    
    
    sprintf(buffer,"%d,",u32Result);
    UART_Write(UART1,buffer,strlen(buffer));
    //UART_Write(UART1,u32Result,1);
    
    
    
    
    return u32Result;
    
    
    }

     

    The code does not show the main loop. But I think it's calling adc_sine continuously

     

    It's initialising , setting the reference of the ADC each time and kicking it off in continuous mode.

    It says it samples continuously, but a single sample is taken then formatted into a string and  sent out to the serial bus (commented out test code says at speed 9600).

    It's going to be too slow. I think it's too slow without the UART write too.

     

    Everything before this line should not be in the loop:

    u32Result = ADC_GET_CONVERSION_DATA(ADC, 1);

     

     

    The writing to the UART should be made efficienter too. Maybe gather a series of samples in a uint32_t buffer (controlled by a timer tick?), then writing when done sampling (I don't know if the display has time as horizontal axis, or measurement count ...)

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 6 years ago in reply to Jan Cumps

    He's using sprintf with %d, so not sending the number, but an ASCII representation. I don't know what his serial plotter is doing, but maybe it is mashing up the characters into nonsense words or long words. Also could be an endian issue or anything. Hardly any info : (

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 6 years ago in reply to Jan Cumps

    Just out of curiosity I tried seeing what ASCII digits and dots and the comma he's got in that string (it is "%d, ") would look like decoded as an integer.

    Any 4 of those range of ASCII characters, seems to give values of the order of 10^8. e.g. "12, " gives 8e8. I wonder if his serial plotter is trying to interpret the stream as a load of 32-bit ints, or something like that..

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 6 years ago in reply to Jan Cumps

    Just out of curiosity I tried seeing what ASCII digits and dots and the comma he's got in that string (it is "%d, ") would look like decoded as an integer.

    Any 4 of those range of ASCII characters, seems to give values of the order of 10^8. e.g. "12, " gives 8e8. I wonder if his serial plotter is trying to interpret the stream as a load of 32-bit ints, or something like that..