Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum reproducing sine wave accurately
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 4 answers
  • Subscribers 502 subscribers
  • Views 1372 views
  • Users 0 members are here
  • cortex-m0 mcu
Related

reproducing sine wave accurately

gnsh
gnsh over 6 years ago

I am using a cortex M0 microcontroller. i am giving a  sine wave input of 1 Hz. this input signal is given to a 12 bit adc and this converted data is given to uart This uart data Im plotting through a serial plotter. image

 

 

how to get a smooth sine wave? from the uart data.

Attachments:
SINEWAVE.c.zip
  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 6 years ago +4 suggested
    So many things could be wrong that it's hard to know where to start suggesting. What does you code do, and where did it come from. How fast are you sampling, how is the data being presented to the UART…
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to michaelkellett +3 suggested
    I found this function in the attachment: int32_t adc_sine(void) { int32_t u32Result; unsigned char buffer[20]; ADC_Open(ADC, ADC_INPUT_MODE_SINGLE_END, ADC_OPERATION_MODE_CONTINUOUS, ADC_CH_1_MASK);…
  • shabaz
    shabaz over 6 years ago in reply to Jan Cumps +3
    He's using sprintf with %d, so not sending the number, but an ASCII representation. I don't know what his serial plotter is doing, but maybe it is mashing up the characters into nonsense words or long…
Parents
  • aspork42
    0 aspork42 over 6 years ago

    Hello,

     

    Could you open a serial monitor program (i.e. PuTTY) and show us what it is sending? I'm willing to bet that the issue is on the side of SerialPlot. I had never heard of SerialPlot, but it is super useful! Now I don't have to use Processing to create simple charts.

     

    I was able to recreate some semblance of your setup with a 1hz sine wave. I'm using an arduino MKR 1010 with its onboard ADC. I think the trick was in how i sent data out the port, then how I asked SerialPlot to display it. I was able to get a cleanish sine wave recreated; although it didn't work until I had gone into the "Data Format" tab and chose ASCII.

    image

     

    Any incorrect setting would result in a garbage plot that didn't reflect the actual data.

     

    This is what my data look like on the serial port:

    image

     

    Sampling at 10Hz:

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • aspork42
    0 aspork42 over 6 years ago

    Hello,

     

    Could you open a serial monitor program (i.e. PuTTY) and show us what it is sending? I'm willing to bet that the issue is on the side of SerialPlot. I had never heard of SerialPlot, but it is super useful! Now I don't have to use Processing to create simple charts.

     

    I was able to recreate some semblance of your setup with a 1hz sine wave. I'm using an arduino MKR 1010 with its onboard ADC. I think the trick was in how i sent data out the port, then how I asked SerialPlot to display it. I was able to get a cleanish sine wave recreated; although it didn't work until I had gone into the "Data Format" tab and chose ASCII.

    image

     

    Any incorrect setting would result in a garbage plot that didn't reflect the actual data.

     

    This is what my data look like on the serial port:

    image

     

    Sampling at 10Hz:

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer