Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Unable to handle kernel paging request at virtual address f09e0000
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 502 subscribers
  • Views 2506 views
  • Users 0 members are here
  • mipi
  • petalinux
  • zybo z7
  • mipi drivers
  • pcam 5c
Related

Unable to handle kernel paging request at virtual address f09e0000

vision3daerospace
vision3daerospace over 5 years ago

Hello all,

 

I am trying to capture images using Zybo PCam , I am using vivado design and petalinux project from digilent as reference. The reference project is in v2017.4 I am trying to implement that in v2019.1

After this the media device is probed and I am successful in getting media graph as well.

 

However after I set the media bus formats and resolution using media-ctl commands, when I try to capture images using the command as shown below I get an error and petalinux freezes.

 

Header 1
media-ctl -d /dev/media0 -V '"ov5640 2-003c":0 [fmt:UYVY/'"640x"480'@1/30' field:none]'
media-ctl -d /dev/media0 -V '"43c60000.mipi_csi2_rx_subsystem":0 [fmt:UYVY/'"640x"480'@1/30' field:none]'
v4l2-ctl -d /dev/video0 --set-fmt-video=width="640",height="480",pixelformat='YUYV'
yavta -c14 -f YUYV -s 640x480 -F /dev/video0

 

The following is the error I get before it freezes.

 

Header 1
 

root@Zybo_ImageSaver:~# yavta -c1 -f YUYV -s 640x480 -F /dev/video0

Device /dev/video0 opened.

Device `vcap_mipi output 0' on `platform:vcap_mipi:0' is a video output (without mplanes) device.

Video format set: YUYV (56595559) 640x480 field none, 1 planes:

* Stride 1280, buffer size 614400

Video format: YUYV (56595559) 640x480 field none, 1 planes:

* Stride 12Unable to handle kernel paging request at virtual address f09e0000

80, buffer size 614400

8 buffers requested.

length: 1 offset: pgd = (ptrval)

3201174072 timestamp type/source: mono/EoF

Buffer 0/0 m[afp0p9ee0000] *pgd=2fffb841, *pte=00000000, *ppte=00000000

at address 0xb6daf000.

length: 1 offset: 3201174072 timestamp Internal error: Oops - BUG: 827 [#1] PREEMPT SMP ARM

type/source: mono/EoF

Buffer 1/0 mappMeodd ualte sa dldirneksesd in: uio_pdrv_genirq

0xb6d19000.

length: 1 offset: 3201174C0P7U2:  t1i mPeIsDt:a m1p318 Comm: yavta Not tainted 4.19.0-xilinx-v2019.1 #1

type/source: moHnaor/dEwoaFr

e

Bnuafmfee:r  X2i/l0i nmxa pZpyend Platform

at address 0xb6c83000.

length: 1 offset: 3201174072 tiPmCe sits at xcsi2rxss_s_stream+0x84/0x1a0

mp type/source: mono/EoF

Buffer 3/0 mapLpRe di sa ta ta dadrrme_heavy_mb+0x18/0x4c

s 0xb6bed000.

lengtphc:  :1  [o<fcf0s5e1t1:1 3302>0]1 1 7 4 0l7r : [<c01146f4>]    psr: 60070013

timestamp type/sourcsep:  :m oeneoa/4E7ocF3

0

B uifpf e:r  e4f/f4110  fp : 006080c0

0 mapped at addressr 100x:b 6ebf517408050c.0

 

lre9n g:t he:f 316944  r8 : 00010000

offset: 3201174072 timre7s t:a mepf 3t4y6p6e7/8s o urr6c e::  em346410  r5 : f09e0000  r4 : ef346460

ono/EoF

Buffer 5/0 marp3p e:d  0a0t0 0a0d0d0r2e s sr 20 x:b 6eae8eb524  r1 : 00000000  r0 : f080a730

1000.

length: 1 offset: F3l2a0g1s1:7 4n0Z7C2v  t iImReQsst aomnp FIQs on  Mode SVC_32  ISA ARM  Segment none

type/source: mono/EoF

CBounftfreorl :6 /108 cm5a3p8p7edd   aTtable: 2e61804a  DAC: 00000051

address 0xb6a2b000.

lenPgrtohc:e s1s  oyfafvsteat image p3i2d0:1 11318, stack limit = 0x(ptrval))

4072 timestamp type/soSutraccek::  m(o0nxoe/eEao4F7

c

3B0u ftfoe 0xeea48000)

7/0 mapped at address 0xb6995000.

7c20:                                     fffffdfd 00000001 ef346460 ef346810

7c40: ef346810 c050c2bc eea47c68 ef148300 c0a03c48 00000000 ef346810 c050c510

7c60: 00010001 ef345018 ef148300 ef1485c0 00000000 00000000 ef345018 ef345048

7c80: ef346460 ef346490 ef353014 ef353044 effd0940 80070013 00000001 effd0940

7ca0: 2ee9c000 c01c1ba4 ffffe000 fffffffc 00000001 c0116b9c c0a346c0 00000000

7cc0: c0a346c0 c01a7c0c c0a03c48 00096000 00000001 eea47d74 00000034 c0a34dc0

7ce0: 0000000f 00000001 f091003c c0380290 ef148940 00000020 00000000 5f46fc1c

7d00: ef288cd0 ef345010 ef34535c 00000000 00000000 ef3453ec ef345010 ef346a3c

7d20: ef345018 c050d13c c0a03c48 ef346810 c0a03c48 00000001 00000000 00000280

7d40: 000001e0 0000200f 00000001 00000008 00000000 00000000 00000000 00000000

7d60: 00000000 00000000 00000000 ef345010 ef345010 eea9a600 eeb09f00 c0a03c48

7d80: ef34563c c050c0d4 eea47e5c 5f46fc1c 00000001 ef345500 ef3454d8 ef3455fc

7da0: c0a26e20 ef345414 eea47e5c c0769b18 c04efd84 c05021f8 00000000 ef345500

7dc0: 40045612 c0a26e20 ef345414 c05034b4 00000001 ef345018 40045612 c04f3b34

7de0: b6a00000 b6a2b000 b6a2b000 eea21500 00000000 ef21cc00 c0a03c48 eea21500

7e00: 00000114 00096000 ef19ea10 5f46fc1c ef19ea10 5f46fc1c bece05cc 00000000

7e20: 00000000 ef21cc00 00000000 40045612 eea47e5c 00000004 00000000 c04f4124

7e40: 00000000 bece07b8 ef21cc00 00000001 c04f3928 00000000 00000000 00000009

7e60: 00000009 00000000 00002003 00000000 00000000 00000000 00000000 00000000

7e80: 00000000 00000000 00000000 00000001 bece05cc 00000001 00000000 00000000

7ea0: 00000001 c038aebc ef21cc00 c038d0cc 00000051 eea27400 ee82a380 eeaebd80

7ec0: c038acbc 00000000 c0a03c48 becde2b0 00000029 00000004 bece092c 5f46fc1c

7ee0: 00096000 bece07b8 ef34acb0 ef21cc00 40045612 bece07b8 eea46000 00000036

7f00: c0a03c48 c01f34f0 bece07b8 c01f3d60 fff69fff 00000000 00000000 00000000

7f20: 00000000 5f46fc1c ef21cc00 eeaebd80 00000000 00000029 eeaebd88 ef116e40

7f40: 00000002 00000004 bece092c c01e3944 00000000 00000000 00000029 eeaebd80

7f60: becde2b0 5f46fc1c eeaebd80 ef21cc00 00000003 ef21cc00 40045612 bece07b8

7f80: eea46000 00000036 bece092c c01f4538 00498f2c b6f9a900 00096000 00000036

7fa0: c0101204 c0101000 00498f2c b6f9a900 00000003 40045612 bece07b8 2a7e4900

7fc0: 00498f2c b6f9a900 00096000 00000036 bece08e8 00000000 0049a4b4 bece092c

7fe0: 00498f64 bece07ac 00486c65 b6efad68 20070030 00000003 00000000 00000000

[<c0511130>] (xcsi2rxss_s_stream) from [<c050c2bc>] (xvip_entity_start_stop+0xcc/0x210)

[<c050c2bc>] (xvip_entity_start_stop) from [<c050c510>] (xvip_pipeline_start_stop+0x110/0x1b0)

[<c050c510>] (xvip_pipeline_start_stop) from [<c050d13c>] (xvip_dma_start_streaming+0x250/0x2b4)

[<c050d13c>] (xvip_dma_start_streaming) from [<c05021f8>] (vb2_start_streaming+0x64/0xec)

[<c05021f8>] (vb2_start_streaming) from [<c05034b4>] (vb2_core_streamon+0xe0/0x13c)

[<c05034b4>] (vb2_core_streamon) from [<c04f3b34>] (__video_do_ioctl+0x20c/0x320)

[<c04f3b34>] (__video_do_ioctl) from [<c04f4124>] (video_usercopy+0x3c4/0x4e4)

[<c04f4124>] (video_usercopy) from [<c01f34f0>] (vfs_ioctl+0x20/0x38)

[<c01f34f0>] (vfs_ioctl) from [<c01f3d60>] (do_vfs_ioctl+0x90/0x830)

[<c01f3d60>] (do_vfs_ioctl) from [<c01f4538>] (ksys_ioctl+0x38/0x54)

[<c01f4538>] (ksys_ioctl) from [<c0101000>] (ret_fast_syscall+0x0/0x54)

Exception stack(0xeea47fa8 to 0xeea47ff0)

7fa0:                   00498f2c b6f9a900 00000003 40045612 bece07b8 2a7e4900

7fc0: 00498f2c b6f9a900 00096000 00000036 bece08e8 00000000 0049a4b4 bece092c

7fe0: 00498f64 bece07ac 00486c65 b6efad68

Code: e0855008 f57ff04e ebf00d6b e3a03002 (e5853000)

---[ end trace 33f6bc73415560a9 ]---

Your help and time is highly appreciated.

Thank you!