Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Which is the new bottleneck of SSD(Solid state Disk)?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 504 subscribers
  • Views 568 views
  • Users 0 members are here
  • ssd
  • nand_flash
  • mlc
  • NVRAM
  • slc
Related

Which is the new bottleneck of SSD(Solid state Disk)?

Oliver
Oliver over 17 years ago

At present, SSD technology is based on Nand Flash(SLC or MLC).


Which is the new bottleneck of it?
Price per GB? Random write control by firmware and driver? or others


What is the next storage IC? NVRAM, Phase-Change RAM,Spin Torque RAM, or Ferroelectric Nand Flash?

  • Sign in to reply
  • Cancel
Parents
  • Michael
    0 Michael over 17 years ago
    SSD is definitely a technology with a bright prospect, with numbers of advantages such as faster write/read rate, invulnerable to shock, smaller size comparing with conventional hard drive, it is likely to be the next generation of data storage. But, to achieve the goal, there are still many obstructions to overcome, and I guess that would probably take more than 5 years until SSD turns out to be a mature technology.
    The biggest problem is the maximum write/read times; so far it can only endure 10,000 to 100,000 times of write/read, if we assume that there are 100 times per day, the longest life will be 1000 days, in other words, the service life of SSD is less than 3 years. Obviously it is too short to serve as data storage.
    The second problem is the price. Currently the price per GB of SSD is awfully higher than that of HD, while the capacity per disk of HD now is up to 640G, and I believe that 1TB is very possible to achieve soon or later with a reasonable price.

    So there is a long way to go for SSD.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • Michael
    0 Michael over 17 years ago
    SSD is definitely a technology with a bright prospect, with numbers of advantages such as faster write/read rate, invulnerable to shock, smaller size comparing with conventional hard drive, it is likely to be the next generation of data storage. But, to achieve the goal, there are still many obstructions to overcome, and I guess that would probably take more than 5 years until SSD turns out to be a mature technology.
    The biggest problem is the maximum write/read times; so far it can only endure 10,000 to 100,000 times of write/read, if we assume that there are 100 times per day, the longest life will be 1000 days, in other words, the service life of SSD is less than 3 years. Obviously it is too short to serve as data storage.
    The second problem is the price. Currently the price per GB of SSD is awfully higher than that of HD, while the capacity per disk of HD now is up to 640G, and I believe that 1TB is very possible to achieve soon or later with a reasonable price.

    So there is a long way to go for SSD.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer