Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Thought Experiment; Detecting Distance
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 37 replies
  • Answers 5 answers
  • Subscribers 506 subscribers
  • Views 3644 views
  • Users 0 members are here
  • embedded
  • development
  • mcu
  • puzzle
Related

Thought Experiment; Detecting Distance

Catwell
Catwell over 16 years ago
We have two blocks, A & B shown below, moving away from each other. How can one detect that the separation has reached a certain point, distance X in this case?
 
The most obvious solution is two rods, one on each block, that make contact when the distance is X. But this is a crude and cumbersome option. It's 2010, how about a high tech solution?

image

 
 
There is no right or wrong, just an excellent chance to work out the prefrontal cortex and showing off some creativity.
  • Sign in to reply
  • Cancel

Top Replies

  • DAB
    DAB over 14 years ago +1
    Hi Cabe, A very simple approach is to set up two laser pointers set up to hit the same spot at only the correct distance. As you move one box towards the other, the two laser spots will converge. If you…
Parents
  • DAB
    0 DAB over 14 years ago

    Hi Cabe,

     

    A very simple approach is to set up two laser pointers set up to hit the same spot at only the correct distance.  As you move one box towards the other, the two laser spots will converge.  If you move them away, the spots diverge.  The approach is simple, you can reset the distance to just about any range where the laser spots are still visible and best of all, its nearly fool proof.

     

    By the way, the British used a similar system to set the altitude for thier bombers when they bombed the Ruhr river dams in Germany.

     

    Thanks

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • DAB
    0 DAB over 14 years ago

    Hi Cabe,

     

    A very simple approach is to set up two laser pointers set up to hit the same spot at only the correct distance.  As you move one box towards the other, the two laser spots will converge.  If you move them away, the spots diverge.  The approach is simple, you can reset the distance to just about any range where the laser spots are still visible and best of all, its nearly fool proof.

     

    By the way, the British used a similar system to set the altitude for thier bombers when they bombed the Ruhr river dams in Germany.

     

    Thanks

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • billpenner
    0 billpenner over 14 years ago in reply to DAB

    Hey DAB

    I like this approach! This way the lasers can be mounted on the extreme of the outside of block A and the stability of block B is not as much a problem.

    The distance is simple to calculate (displacement of dots). However, there is no way to calculate the negative, since a distance beyond the convergence of the dots will be the same result as the positive. For a little more sophistication a linear diode array mounted on block B would provide a direct readout of distance.

    Bill

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • billpenner
    0 billpenner over 14 years ago in reply to DAB

    DAB

    Another thought... if plus/minus is imporant , two different color lasers and filters on the linear arrays would allow diferentation of plus & Minus.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • DAB
    0 DAB over 14 years ago in reply to billpenner

    Hi Bill,

     

    It would be easier to just use a video camera and compare the dot positions from frame to frame.  That way you get both position and direction for each laser pointer.  Remember, Keep It Simple if you want something to work.

     

    Thanks,

    DAB