Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum How do you monitor the power conversion from AC to DC in applications such as Solar Micro Inverters?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 502 subscribers
  • Views 613 views
  • Users 0 members are here
  • freescale
  • micro
  • inverters
  • high
  • supplies
  • power
  • solar
Related

How do you monitor the power conversion from AC to DC in applications such as Solar Micro Inverters?

MAb
MAb over 15 years ago
It's a key challenge to monitor and accurately control the power conversion from AC to DC in applications such as solar micro inverters because of safety and reliability in high voltage applications.
 
Actually, as you are dealing with very high, hence dangerous voltages it is  critical to be able to control any ramp up and ramp down and the voltage  range. it's also important to be able to monitor that effectively so you can detect  any issue and shut down in case of any issue to avoid a major incident. That's the case of high voltage power supplies
 
So how do you manage that ?
  • Sign in to reply
  • Cancel
Parents
  • Catwell
    0 Catwell over 15 years ago

    Texas Instruments has a whole line of AC-DC monitoring solutions. See here.

     

    And Freescale has the same.

     

     

    Also, the Enphase Solar Micro Inverter system is monitorable via the internet. You may not have to build it at all.

     

    However, what is your application?

     

    Cabe

     

     

    However, what is your application?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • MicrochipRTCfr
    0 MicrochipRTCfr over 15 years ago in reply to Catwell

    Hi,

     

    You may also download complete packages of Micro Inverter reference designs from Microchip for 100V & 220V here.

     

    Regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • MicrochipRTCfr
    0 MicrochipRTCfr over 15 years ago in reply to Catwell

    Hi,

     

    You may also download complete packages of Micro Inverter reference designs from Microchip for 100V & 220V here.

     

    Regards