Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Use of stimulus on Microchip MPLAB SIM query
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 503 subscribers
  • Views 731 views
  • Users 0 members are here
Related

Use of stimulus on Microchip MPLAB SIM query

cityswift
cityswift over 15 years ago

Hi - does anyone know if is possible to use the stimulus tool on this simulator to inject an asynchronous 1Hz square wave signal into the Timer0 signal input pin on a 16F630 microcontroller? I have tried studying the help content on this tool but cannot make sense of it. It only gives a very sketchy description of the setting up of a test file. Considering that one can inject a series of controlled inputs into a register, I would have thought that my requirement was simple. Have I missed something obvious? Any comment would be appreciated.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    MPLAB SIM does offer clock stimulus option, and can be set a wide range of frequency and duty cycles as a function of cycles.

    The "cycle" refers to instruction cycles. Since the 8 bit PIC micro has four Fosc system clocks for every instruction cycle, a 4 MHz Fosc will produce 1 MIPS operation.


    Referring to PIC16F630 datasheet FIGURE 4-1: BLOCK DIAGRAM OF THE TIMER0/WDT PRESCALER,  an external input is available on the T0CKI pin with T0CON<bit5>, T0CS, TMR0 Clock Source Select bit  equal to 1. However, T0CON<PS2:PS0>, Prescaler Rate Select bits, equal to 000'b is 1:2, requiring the input twice the frequency as the desired interrupt rate. Therefore, the simulator clock input will two times the desired timer 0 overflow rate.

    As a result, the simulators clock stimulus will be 2 Hz, on T0CKI/RA2 pin, with 250000 cycles on low and high cycle count perameter.

    There in an asynchronous  input option on the simulator, but the clock stimulus is synchronous by nature of a clock operation.

    Hope all this helps ?

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • cityswift
    0 cityswift over 15 years ago in reply to e14 Contributor

    Hi Mike thanks for your prompt reply from which I gather there is no provision in the simulator for the generation of asynchronous pulse patterns. What I will do is  hit the "fire" button on the asynchonous tab sheet 300 times in 5 minutes and that will give me the simulation I need.