Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Sending signals as current vs voltage, advantages?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 503 subscribers
  • Views 507 views
  • Users 0 members are here
  • signal
  • trace
  • microprocessor
  • microcontrollers
  • anolog
  • sensor
Related

Sending signals as current vs voltage, advantages?

ZeroSizeObject
ZeroSizeObject over 15 years ago
If you are sending a signal through a PCB to a microcontroller, what is the preferred way to send it, current or voltage? What are the advantages and disadvantages of using either?
 
I ask because I have a signal that is corrupted would be quite devastating in the overall purpose of the device. I have experience more noise with the voltage based signal. And if I can not shorted the traces between the sensor (anolog) to the microcontroller, that is the better option?
 
Zero
  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    As usally the world is not digital, hard to tell a absolute truth. But as you said, shorter traces will create less antennas to pick up noise.

    Current drive has a lot of benefits. Specially in generated noise. If you connect a current source to a virtual gnd input, ther will be no

    rise or fall times that can create any transients as the voltage is about zero.

    A current input also normaly need more energy in the noise signal to be disturbed.(also depends on impedans and input sensitivety)

    You can keep a voltage signal in good condition too if you have a low impedans source and low impedans input, but that will add

    some current consumption. If it is a slow signal you also may put some capacitive decoupling?

    Another way is to use a balanced signal that will make the imunity much better.

    Best regards

    /Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jvdberg@ieee.org
    0 jvdberg@ieee.org over 15 years ago in reply to e14 Contributor
    Zero,
     
    If you are sending a signal from one side of a PCB to the other side, noise should not be a problem, unless the design of the PCB is poor and crosstalk between circuits is occurring.
     
    For sending weak signals over some distance in a noisy environment, a current loop over a balanced line is the best solution.
     
    Between an analog sensor and a digital system there should be an interface. Part of this interface could be a filter to separate the wanted signal from the noise.
    The interface should be located as close to the sensor as possible, to prevent interference,

    A digital signal between the interface and the microcontroller is less sensitive for noise

     

    If the sensor is using a different powersupply than the controller, the wires to the sensors powersupply could pick up a lot of noise.

    Sending the data via an optocoupler to the controller could help in that case.