Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Embedded WiFi recommendations?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 34 replies
  • Answers 2 answers
  • Subscribers 505 subscribers
  • Views 5033 views
  • Users 0 members are here
  • wifi
  • 802.11
  • embedded
  • microcontroller
  • wireless
  • arduino
Related

Embedded WiFi recommendations?

fustini
fustini over 15 years ago

Howdy,

 

I was wondering if anyone might have recommendations for WiFi modules for a low-end embedded system.  I'm primarily thinking of Arduino so a simple interface to the radio would be ideal (not USB).

 

Thanks,

Drew

  • Sign in to reply
  • Cancel

Top Replies

  • PBrunner
    PBrunner over 15 years ago in reply to e14 Contributor +1 suggested
    You are perfectly right Julian Freescale has actually 3 different Wifi modules based on 3 different chipsets from 3 different suppliers( http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=0152106740AFE4…
  • e14 Contributor
    e14 Contributor over 14 years ago +1
    There is also TI CC3000 which is a UART-to-WIFI module, probably a more compact solution with respect to the MCW1001A+MRF24WB0Mx couple. Although I've used the Microchip's one in a dev-kit of theirs and…
  • Funklord
    Funklord over 14 years ago +1
    The Microchip MRF24WBOMx modules are great, especially due to the low price, and existing code for 8bit PIC, AVR and Arduino etc. I'm successfully using it with an ATMEGA168 (or better) and WPA2/AES encryption…
Parents
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    Do you want a module that does serial link to wifi conversion, or do you want to run a TCP/IP stack on your controller?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • fustini
    0 fustini over 15 years ago in reply to e14 Contributor

    Hi Julian,

     

    Ideally, I'd like a TCP/IP interface so that the embedded system could directly access Internet content (like a RSS feed).  But now that you've raised the question, I'm not sure the Arduino (8-bit AVR) could handle a TCP/IP stack and higher level protocols, so I'm not opposed stepping up to a beefier MCU like PIC32 or ARM Cortex-M3. 

     

    The most important factors for the system are low-cost & low-power.  I know there's buckets of cheap USB wi-fi modules out there, but I suspect I'd have to upgrade to a more costly & power hungry system capable of running Linux to use them.

     

    Thanks,

    Drew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to fustini

    I've managed to get a TCP/IP stack plus WiFi drivers running on a PIC18 (also 8 bit) so don't give up hope.  And I managed to port it to AVR, if I recall rightly.  If you'd like to see the code, let me know.

     

    Otherwise, Microchip do a rather nice (and cheap) WiFi module (http://www.microchip.com/stellent/idcplg?IdcService=SS_GET_PAGE&nodeId=1406&dDocName=en549227) which you control via SPI, and their TCP/IP stack is pretty standardised and should be easy to port.

     

    J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • fustini
    0 fustini over 15 years ago in reply to e14 Contributor

    Thanks for the suggestion - I'll check out that Microchip part.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to fustini

    If you do want to branch out, I'd also recommend looking at Freescale's Tower System, for which there are a number of WiFi modules (with free software drivers and stacks).  E.g. http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=TWR-WIFI-AR4100.  Plus, the Kinetis Cortex-M4 processors are pretty awesome, and there's a full free RTOS for them too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to fustini

    If you do want to branch out, I'd also recommend looking at Freescale's Tower System, for which there are a number of WiFi modules (with free software drivers and stacks).  E.g. http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=TWR-WIFI-AR4100.  Plus, the Kinetis Cortex-M4 processors are pretty awesome, and there's a full free RTOS for them too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • PBrunner
    0 PBrunner over 15 years ago in reply to e14 Contributor

    You are perfectly right Julian Freescale has actually 3 different Wifi modules based on 3 different chipsets from 3 different suppliers(http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=0152106740AFE4) . This allows you to select the one that is meeting your specification requirements while they are all supported into the Tower ecosystem. This opens you up the access to the Kinetis 32 bits MCUs but also to the 8 bits MCU that are also supported by this dev tool. And to MQX which is a very complete and FREE OF CHARGE RTOS.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer