Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum SuperSpeed USB - How much is it actually?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 1 reply
  • Answers 1 answer
  • Subscribers 502 subscribers
  • Views 328 views
  • Users 0 members are here
  • superspeed
  • usb
  • altera
  • performance
Related

SuperSpeed USB - How much is it actually?

ngadhia
ngadhia over 14 years ago

I have seen a number of articles mentioning SuperSpeed IP sales and  various performance numbers (only theoretical).  I would like to use  this platform to inform the users the actual speed achieved on USB 3.0 Development board by IP designers at SLS

The  core efficiency is dependent on a number of factors like 8b/10b    encoding, packet structure and framing, link level flow control and    protocol overhead.

At   5Gbps signalling rate with 8b/10b encoding, the raw throughput is    500MBps.  When link flow control, packet framing, and protocol overhead    are considered, it is realistic for 400MBps or more to be delivered  to   an application.

Various tests performed with SLS SuperSpeed USB core on GigaByte A75 Motherboard have indicated the performance ~2.1Gbps  with mass storage interface and ~2.7Gbps with raw interface.

 

Any other experiences with the speed/performance of SuperSpeed cores are most welcome!

Attachments:
imagebr_dbusb30_r2a_1.0.pdf
imagebr_usb30sf_1.1_1.3.pdf
  • Sign in to reply
  • Cancel
  • DAB
    0 DAB over 14 years ago

    The true data rate on any connection depends upon several things.

    Protocol

    Error detection and correction

    Data buffering speed on both sides of the connection

    Direct memory access

    memory and cache speeds

    software and firmware speeds

     

    I could go on, but the main message I want to leave here is that you need to look at your entire system components before you can determine your best run time speeds.  I have seen several 100 Mbps links that could only support about 10 Mbps after you threw in the above conditions.

    Bottom line, build a nice timing simulation and check out the real capabilities of your system components, both hardware and software.  If you just trust the specification sheets, you will end up with timing problems.  I know, this was my specialty for a large number of years.  I built my own system simulation software and helped different customers find a lot of hidden timing problems within their system.

    Trust but verify.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer