Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum how to generate 50to 60 hz sine wave from pwm
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 2 answers
  • Subscribers 504 subscribers
  • Views 2420 views
  • Users 0 members are here
  • c
  • microprocessor
  • answer
  • embedded_system
  • embedded
  • electronics
  • software
Related

how to generate 50to 60 hz sine wave from pwm

e14 Contributor
e14 Contributor over 12 years ago

I Want to know that how to generate the 50 -60 hz frequency by using pwm . If any body have any idea about then please tell me .

  • Sign in to reply
  • Cancel

Top Replies

  • kas.lewis
    kas.lewis over 8 years ago +2 suggested
    https://www.youtube.com/watch?v=qVeERT4nyz8 This may be a helpful and informative video, I sure found it to be so. Kas
  • dougw
    dougw over 12 years ago in reply to e14 Contributor +1
    Hi Rahil, You could start by trying something like this which generates a slow triangle wave: PWM Signal Generation using AVR Timers Then shorten the timing until the brightness loop is ramping up and…
  • valiza
    valiza over 8 years ago in reply to sarah123 +1 suggested
    Can't just give you the full code but I will give you hints. Configure TimerCounter1 (TCCR1A and TCCR1B) to give a PWM of >6khz. Make a array of sine wave values with the resolution you want (100 in this…
Parents
  • dougw
    0 dougw over 12 years ago

    Hi Rahil,

    PWM can be converted to voltage using a lowpass filter - a simple R-C can be enough. To generate a sinusoidal voltage at such a filter the pulse width must be modulated sinusoidally.

    pulse width = sine (time) * MaxPulseWidth

    Time can be a simple count that increments with time. The increments must occur at a rate that forces the sine of the count to roll over to the same value 120 times per second. For example the sine of 360 degrees is the same as 0 degrees or 180 degrees or 720 degrees. So you could make the counter increment at a rate of 360 steps in 1/60th of a second. You can also reset the count when it reaches 360. The sine of the count will vary from 0 to 1, so it must be multiplied by the maximum pulse width before being sent to your PWM generator.

    Note that the frequency of the PWM signal should be much higher than the 60 Hz you are trying to create and the lowpass filter should have a cutoff frequency above 60 Hz.

    Doug

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to dougw

    Sir thank you for your  reply . But i have another question about it that if I want to generate a 50 -60 hz freq. form atmega 16 then how can I do it ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to dougw

    Sir thank you for your  reply . But i have another question about it that if I want to generate a 50 -60 hz freq. form atmega 16 then how can I do it ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • dougw
    0 dougw over 12 years ago in reply to e14 Contributor

    Hi Rahil,

    You could start by trying something like this which generates a slow triangle wave:

    PWM Signal Generation using AVR Timers

    Then shorten the timing until the brightness loop is ramping up and down 60 times per second. (60 Hz triangle wave)

    Replace the resistor with 10 Kohm and the LED with a 1 microfarad capacitor and measure the voltage waveform across the capacitor.

    Then replace the "brightness" values with sinusoidal values instead of triangle wave values.

    Doug

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    hi

    2 things . all the info Doug provided are completely correct and precise(as a matter of fact I was going to mention the filtering of a square wave by LP filter)

    another thing is if you have atmega16 (as far as I know it has DAC) why you are going to use timer/pwm method instead of DAC?!