Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Guidance for 12 yrs old to get started with embedded HW/SW projects
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 2 answers
  • Subscribers 504 subscribers
  • Views 838 views
  • Users 0 members are here
  • embedded
Related

Guidance for 12 yrs old to get started with embedded HW/SW projects

e14 Contributor
e14 Contributor over 12 years ago


Hello,

 

My 12yrs old son wants to do projects in embedded HW/SW domain. He is just beggining to explore the embedded domain. I am trying to help him get started. I am looking for a simple 8/16 bit microcontroller evaluation board with basic digital input/output, LEDs, LCD display, A/D, D/A converters, external memory, an IDE where he can write simple programs in C/C++ compile, download via USB and execute. Can you please suggest the right product/s  I need to buy for him?

 

Thanks

Radhakrishna

  • Sign in to reply
  • Cancel

Top Replies

  • Problemchild
    Problemchild over 12 years ago +1
    Hi Sriram your son is obviously at the entry point of this technology I would take note of the advice given here which so far sounds most reasonable and then to be honest it does not really matter which…
Parents
  • vsluiter
    0 vsluiter over 12 years ago

    The xplained boards for the Atmel Xmega series are very nice, and some (like the one for Atxmega256A3BU) have nice demo applications.

    Why limit to 8/16 bit?

    A simple but clear C++ front end can be provided by mbed, which supports several demo boards, with several possibilities. The 'original' LPC1768 board is still nice, especially in combination with the application board (LCD, potmeters, etcetera). Drawback: the price of those two combined is quite  high, in my opinion.

    The KL46z (FRDM-KL46Z | mbed) is nice in that it's cheap, has an LCD and is mbed compatible.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • vsluiter
    0 vsluiter over 12 years ago

    The xplained boards for the Atmel Xmega series are very nice, and some (like the one for Atxmega256A3BU) have nice demo applications.

    Why limit to 8/16 bit?

    A simple but clear C++ front end can be provided by mbed, which supports several demo boards, with several possibilities. The 'original' LPC1768 board is still nice, especially in combination with the application board (LCD, potmeters, etcetera). Drawback: the price of those two combined is quite  high, in my opinion.

    The KL46z (FRDM-KL46Z | mbed) is nice in that it's cheap, has an LCD and is mbed compatible.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer