Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Guidance for 12 yrs old to get started with embedded HW/SW projects
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 2 answers
  • Subscribers 504 subscribers
  • Views 853 views
  • Users 0 members are here
  • embedded
Related

Guidance for 12 yrs old to get started with embedded HW/SW projects

e14 Contributor
e14 Contributor over 12 years ago


Hello,

 

My 12yrs old son wants to do projects in embedded HW/SW domain. He is just beggining to explore the embedded domain. I am trying to help him get started. I am looking for a simple 8/16 bit microcontroller evaluation board with basic digital input/output, LEDs, LCD display, A/D, D/A converters, external memory, an IDE where he can write simple programs in C/C++ compile, download via USB and execute. Can you please suggest the right product/s  I need to buy for him?

 

Thanks

Radhakrishna

  • Sign in to reply
  • Cancel

Top Replies

  • Problemchild
    Problemchild over 12 years ago +1
    Hi Sriram your son is obviously at the entry point of this technology I would take note of the advice given here which so far sounds most reasonable and then to be honest it does not really matter which…
Parents
  • johnbeetem
    0 johnbeetem over 12 years ago

    For 16-bit, though I've never used it personally I really like TI's MSP430 architecture.  There are some inexpensive LaunchPad boards that a great way to get started: http://www.ti.com/lsds/ti/microcontroller/16-bit_msp430/tools_software.page#msp430pad

     

    There's also Arduino, which is very popular though I haven't used it myself.  I'll let others give advice on Arduino.

     

    However, I think these days you're much better off with a 32-bit ARM Cortex board.  There are probably hundreds of these boards out there, with dozens worth considering seriously.  I personally like:

     

    ST Discovery, which have clean IC documentation and it's easy to hook up JTAG or SWD: http://www.element14.com/community/docs/DOC-40220?ICID=knode-devkit

     

    Cypress PSoC 4 and PSoC 5LP: http://www.element14.com/community/docs/DOC-53992?ICID=knode-cypresspioneerkit-space

     

    TI Tiva ARM (haven't used personally): http://www.ti.com/lsds/ti/microcontroller/tiva_arm_cortex/c_series/tools_software.page#ekits

     

    NXP mbed and LPCXpresso (haven't used personally): http://www.nxp.com/techzones/microcontrollers-techzone/tools-ecosystem.html

     

    Freescale Freedom (haven't used personally): http://www.element14.com/community/community/knode/dev_platforms_kits/element14_dev_kits/kinetis_kl2_freedom_board?ICID=knode-devkitroom

     

    My apologies to those I've inadvertently left out.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to johnbeetem

    Thank you so much for your guidance, I will explore the options

     

    Sriram

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Freescale just announced today at their FTF show a bunch of new enablement for the new second gen Kinetis K64F part: mbed enabled freedom board, SDK software framework, and software bootloader (UART, SPI, I2C, USB HID, or CAN). The SDK may be interesting to simplify the coding.


    But any of the Freedom boards would let you get drag and drop programs easily though, and the FRDM-KL46Z would probably be the best one (SLCD as mentioned before, lots of IO, and easy programming/serial over a USB cable).

     

    Hope the embedded bug bites him, it's a fun world to be in image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Freescale just announced today at their FTF show a bunch of new enablement for the new second gen Kinetis K64F part: mbed enabled freedom board, SDK software framework, and software bootloader (UART, SPI, I2C, USB HID, or CAN). The SDK may be interesting to simplify the coding.


    But any of the Freedom boards would let you get drag and drop programs easily though, and the FRDM-KL46Z would probably be the best one (SLCD as mentioned before, lots of IO, and easy programming/serial over a USB cable).

     

    Hope the embedded bug bites him, it's a fun world to be in image