Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum I2C communication between 3.3V uC and 5V uC
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 505 subscribers
  • Views 2459 views
  • Users 0 members are here
  • level_conversion
  • i2c
  • arduino
Related

I2C communication between 3.3V uC and 5V uC

vish
vish over 12 years ago

Hello all,

 

I'm currently working on a project which has a few different microcontroller boards to form a network. I'm planning to use I2C to communicate with each other. But two of my development boards are working on 3.3V range and other boards( arduinos ) are working at 5V range. As I want to use same I2C bus to communicate with them all, what kind of conversion circuit I have to use to interface my 3.3V development boards to I2C bus?

 

Thanks ahead,

vish

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago +1 verified
    The correct way to do it is given here http://www.nxp.com/documents/application_note/AN10441.pdf There are also specific devices designed to do it like http://www.ti.com/product/pca9306 What John alludes…
Parents
  • johnbeetem
    0 johnbeetem over 12 years ago

    I2C devices have open-drain drivers, which only pull the SCL and SDA lines low to 0V.  Each I2C line should have a single pull-up resistor: make sure they pull up to 3.3V and not 5V.  Also make sure that each 5V part has a reasonable Vih (Input voltage high) threshold.  Many 5V chips use TTL Vih which is 2.0V, which works.  Others may have Vih = 0.7 x 5.0 = 3.5V, which means you'll have to do something else.

     

    If you want to make sure 3.3V I2C inputs don't go too high, clamp SCL and SDA to 3.3V with Schottky diodes.  That will limit them to 3.5V or so.  They should not be needed if the SCL and SDA pull-up resistors are connected to 3.3V, but it doesn't hurt and may protect you from killing a board accidentally.

     

    Wikipedia has a good article on I2C: http://en.wikipedia.org/wiki/I2C

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • johnbeetem
    0 johnbeetem over 12 years ago

    I2C devices have open-drain drivers, which only pull the SCL and SDA lines low to 0V.  Each I2C line should have a single pull-up resistor: make sure they pull up to 3.3V and not 5V.  Also make sure that each 5V part has a reasonable Vih (Input voltage high) threshold.  Many 5V chips use TTL Vih which is 2.0V, which works.  Others may have Vih = 0.7 x 5.0 = 3.5V, which means you'll have to do something else.

     

    If you want to make sure 3.3V I2C inputs don't go too high, clamp SCL and SDA to 3.3V with Schottky diodes.  That will limit them to 3.5V or so.  They should not be needed if the SCL and SDA pull-up resistors are connected to 3.3V, but it doesn't hurt and may protect you from killing a board accidentally.

     

    Wikipedia has a good article on I2C: http://en.wikipedia.org/wiki/I2C

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer