Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum I2C communication between 3.3V uC and 5V uC
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 505 subscribers
  • Views 2463 views
  • Users 0 members are here
  • level_conversion
  • i2c
  • arduino
Related

I2C communication between 3.3V uC and 5V uC

vish
vish over 12 years ago

Hello all,

 

I'm currently working on a project which has a few different microcontroller boards to form a network. I'm planning to use I2C to communicate with each other. But two of my development boards are working on 3.3V range and other boards( arduinos ) are working at 5V range. As I want to use same I2C bus to communicate with them all, what kind of conversion circuit I have to use to interface my 3.3V development boards to I2C bus?

 

Thanks ahead,

vish

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago +1 verified
    The correct way to do it is given here http://www.nxp.com/documents/application_note/AN10441.pdf There are also specific devices designed to do it like http://www.ti.com/product/pca9306 What John alludes…
Parents
  • vish
    0 vish over 12 years ago

    hello both,

    thanks a lot for your reply. I just found this article where they are connecting 3v3 rPi to 5V arduino directly for I2C. Thought I might share with you. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • electronichamsters
    0 electronichamsters over 12 years ago in reply to vish

    Probably too late to the discussion.  But there are a lot of Arduino clones that include a 3.3V to 5V switch.  I think that makes them easier to use.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • electronichamsters
    0 electronichamsters over 12 years ago in reply to vish

    Probably too late to the discussion.  But there are a lot of Arduino clones that include a 3.3V to 5V switch.  I think that makes them easier to use.