Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum FTDI - DB9-USB-D3-F - MODULE
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 2 answers
  • Subscribers 504 subscribers
  • Views 1585 views
  • Users 0 members are here
  • usb/rs232
  • ft232r
  • ftdi
Related

FTDI - DB9-USB-D3-F - MODULE

vivi
vivi over 11 years ago

Hello everybody,

have you anyone used DB9-USB-D3-F - FTDI - MODULE, USB TO UART, 1 CH, FT232R | Farnell ? I need them as USB/RS232 converters.. I have bought two modules, but I cant send any data into PC from any of them. If I connect logic analyzer to TXD pin, so I can send data from PC terminal to "logic analyzer" (so FTDI driver should be OK). But when I connect RX to TX (to make a loop), so transmitted data never come back to terminal. I have WIN7.

 

Thanks for any idea..

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 11 years ago in reply to vivi +1
    It looks as if you are up and running now - great. I used to work with an engineer who wouldn't bother to to specify RX and TX because he said that in on average least 50% of cases someone would make a…
Parents
  • vivi
    0 vivi over 11 years ago

    Uf, it already works image There are two possibilities: 1) I am stupid 2) Datasheet is "little" bit confusing. Please tell me, what is correct..

     

    1) I have FEMALE USB bridge

    2) If I connected logic analyzer to pin 3 (red circled), so I could "see" sent data from terminal.

    3) I have connected red circled pins together to make a loop. If the green rectangle stands for PCB, so it seems logically to me, that FTDI bridge must be under the PCB with pins upwards on the picture. I admit, that I have not read the text under the picture. I have expected, that "UART Transceiver" is a part of MCU..

    3) If I connected red circled pin together to make a loop, so nothing came back to terminal => That was my problem.. Till now..

    4) I have connected green circled pins together and every sent data from terminal immediately came back..Loop works !!!

     

    Datasheet can be found here: http://www.farnell.com/datasheets/1812681.pdf   image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • vivi
    0 vivi over 11 years ago in reply to vivi

    Can you draw a little diagram of your set up - I don't understand at all where the RS232 cable comes into things..

     

    Just connected RS232 directly to PC (no FTDI) with connected pins 2 and 3 together (just to verify functionality terminal Hercules)..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • vivi
    0 vivi over 11 years ago in reply to vivi

    Can you draw a little diagram of your set up - I don't understand at all where the RS232 cable comes into things..

     

    Just connected RS232 directly to PC (no FTDI) with connected pins 2 and 3 together (just to verify functionality terminal Hercules)..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • michaelkellett
    0 michaelkellett over 11 years ago in reply to vivi

    It looks as if you are up and running now - great.

     

    I used to work with an engineer who wouldn't bother to to specify RX and TX because he said that in on average least 50% of cases someone would make a mistake wiring  a socket or a lead so you wasted no more time by guessing and saved yourself the hassle of thinking.

     

    The advantage I have had over you is that I've only used the FTDI cables which have nicely un-ambiguous colour coding.

     

    MK