Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum how to connect FPGA with linux
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 2 answers
  • Subscribers 504 subscribers
  • Views 741 views
  • Users 0 members are here
Related

how to connect FPGA with linux

kamtar
kamtar over 11 years ago

Hello,

I was thinking about how to directly connect a FPGA to linux (iMX233 board based on the olimex design).

I have two ideas:

- SPI (maybe with MCU for parallel interface with FPGA and basic data processing).

- External "address translation" system and use few bytes of memory space for some universal parallel interface.


I'm doing it just for myself (universal board for fun) so no special purpose.

Anyone with experience in this? Any tips?


 

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 11 years ago +1 suggested
    On real designs I often do both and a bit more: SPI with a couple of extra handshake lines memory interface, sometimes with full address bus but often with most of the address lines missed off leaving…
  • kamtar
    kamtar over 11 years ago +1
    Thank you, I think that its a good idea to have both, FPGA with parallel data bus. Then MCU and buffer so i can communicate with it directly or over SPI (if i need to use MCU for realtime data processing…
  • johnbeetem
    0 johnbeetem over 11 years ago

    Hi Tomas,

     

    You might also try asking this in the http://www.element14.com/community/groups/fpga-group.

     

    Here's my answer: the beauty of FPGAs is that you can design the FPGA to match whatever interface(s) the board or SoC has available.  The easiest IMO is if the SoC has an external memory bus: the FPGA simply acts as read/write memory.  You can also do SPI and/or I²C.  SPI is faster and simpler than I²C.  If you're really ambitious, you can do PCI or even PCI express.

     

    ValentF(x) has a hardware/software co-design approach for their LOGI boards that might be helpful: http://www.element14.com/community/groups/fpga-group/blog/2014/10/09/hardwaresoftware-co-design-with-the-logi-boards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 11 years ago

    On real designs I often do both and a bit more:

     

    SPI with a couple of extra handshake lines

    memory interface, sometimes with full address bus but often with most of the address lines missed off leaving perhaps A0, A1, A2 and A19,A19 and  a couple of chip selects -  this saves a lot of pins and tracks but if you do blocks of sequential reading or writing it can be very fast.

    It's always good to have a few additional control signals which will save your bacon as the design evolves over time.

     

    I quite like UARTS as well, I've taken to adding debug UARTS to bigger FPGA designs so I can just connect a PC to them via one the FTDI USB to UART bridge 'wires' and talk to them.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • kamtar
    0 kamtar over 11 years ago

    Thank you,

    I think that its a good idea to have both, FPGA with parallel data bus. Then MCU and buffer so i can communicate with it directly or over SPI (if i need to use MCU for realtime data processing).