Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Dual booting hex files
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 2 answers
  • Subscribers 503 subscribers
  • Views 1191 views
  • Users 0 members are here
Related

Dual booting hex files

dr.akshay_1980@yahoo.com
dr.akshay_1980@yahoo.com over 11 years ago

Can I load two different hex files on same microcontroller so that whenever it boots up, It should ask me the option to select. This is samly analogous to booting up my PC with two different operating systems. I want to write new bootloader for it.

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 11 years ago

    Actually this can be done and is used on various embedded boards. Look at the FRDM-K64F, when you plug a micro cable into board, holding the reset button for 30 seconds tells the bootloader to enter different code and act differently. Alas, there is no interface to talk to for the bootloader like a PC has.. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dr.akshay_1980@yahoo.com
    0 dr.akshay_1980@yahoo.com over 11 years ago in reply to clem57

    Hi Clem,

                  Thanks for the reply , indeed happy to learn that this concept is possible in microcontrollers. Now my next task is that modification of lower end microcontroller bootloader in order to work the same way. Is there any possible solution or indirect way to do that. Is there any difference between binary file and the image file which can be burn on the microcontroller. Do  chinese mp5 players uses any kind of operating system on which multiple applications are running such as audio,video,record,ebook etc. Kindly provide as much as details you can.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 11 years ago in reply to dr.akshay_1980@yahoo.com

    Hi Akshay,

     

    I think you're suggesting to have two or more programs stored in flash and a program to select which one you want. It is partially microprocessor/microcontroller-specific. What you're suggesting is no different than what an OS offers. There are plenty of books that explain this, executable file formats, etc. Look for documentation on (say) CP/M and you'll get a good idea how it could work on limited resource devices like microcontrollers. Expect to do some of it in assembly.

    I don't have any more detail - ordinarily one would use an OS if one wanted to do this, such as Linux. I''m not sure deciphering mp3 players is possible,

    at least not unless you have detailed knowledge working for the manufacturer of them.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 11 years ago in reply to dr.akshay_1980@yahoo.com

    Hi Akshay,

     

    I think you're suggesting to have two or more programs stored in flash and a program to select which one you want. It is partially microprocessor/microcontroller-specific. What you're suggesting is no different than what an OS offers. There are plenty of books that explain this, executable file formats, etc. Look for documentation on (say) CP/M and you'll get a good idea how it could work on limited resource devices like microcontrollers. Expect to do some of it in assembly.

    I don't have any more detail - ordinarily one would use an OS if one wanted to do this, such as Linux. I''m not sure deciphering mp3 players is possible,

    at least not unless you have detailed knowledge working for the manufacturer of them.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer