Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum PWM signwave with 50ns freq. Step
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 1 answer
  • Subscribers 503 subscribers
  • Views 1184 views
  • Users 0 members are here
Related

PWM signwave with 50ns freq. Step

e14 Contributor
e14 Contributor over 11 years ago

Hi all,
i want to generate PWM step with 50ns. For this i have input signal.


PWM clock freq. = 24MHz.

 

 

 

if input is 3,25v  then PWM freq = 1 µs (microsec)
if input is 0,5v then PWM freq = 250ns (nanosec).

 

pls share ur ideas for doing this task.

 

Regards
Max

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 11 years ago +1 suggested
    pls wrt n englsh bcs it wll B ezier 2 undrstnd And it really does not take much longer. When you are generating a PWM signal you need to consider two frequencies, the basic clock frequency of the generating…
  • michaelkellett
    michaelkellett over 11 years ago in reply to e14 Contributor +1
    I don't think so ! In a PWM system where one driver pulls the load high and the other pulls it low the deatime is the time when both drivers are off. It's provided by many controllers so that one device…
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    how can i calculate Deadtime??

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Max,

     

    If your min and max values are 3.25V for 24 steps and 0.5V for 2 steps, you will have 22 steps between them, so 3.25V - 0.5V = 2.75V.  Divide by 22 steps and you have 0.125V per step.  That will be a constant.  Read the input voltage, subtract 0.5V, divide that number by 0.125 and that will give you the number of steps.  125ns + (40ns * # of steps) = Total Dead Time.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 11 years ago in reply to e14 Contributor

    I don't think so !

     

    In a PWM system where one driver pulls the load high and the other pulls it low the deatime is the time when both drivers are off. It's provided by many controllers so that one device can turn off before the other turns on and thus avoids current going straight through the two devices. (Oftne known a "shoot through" current.)

     

    This link (page 28) has a n explanation and  a diagram.

     

    ww1.microchip.com/downloads/en/DeviceDoc/70062E.pdf

     

    You calculate it according to the precise nature of the controller and you work out what you need either by experiment or simulation/calculation based on the power devices you are using.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 11 years ago in reply to e14 Contributor

    I don't think so !

     

    In a PWM system where one driver pulls the load high and the other pulls it low the deatime is the time when both drivers are off. It's provided by many controllers so that one device can turn off before the other turns on and thus avoids current going straight through the two devices. (Oftne known a "shoot through" current.)

     

    This link (page 28) has a n explanation and  a diagram.

     

    ww1.microchip.com/downloads/en/DeviceDoc/70062E.pdf

     

    You calculate it according to the precise nature of the controller and you work out what you need either by experiment or simulation/calculation based on the power devices you are using.

     

    MK