Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum What would I use for this function in a circuit?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 2 answers
  • Subscribers 503 subscribers
  • Views 711 views
  • Users 0 members are here
  • control
  • motor
Related

What would I use for this function in a circuit?

e14 Contributor
e14 Contributor over 11 years ago

If I were to have a motor, and stopped it with my fingers, what component would shut the motor off if it experiences a certain amount of load? This is on a normal DC motor, but i could also use a stepper motor. Thanks! Feel free to ask for more information.

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 11 years ago +1 suggested
    Hi Mathew, I see that Doug has covered things very well while I was drawing up this circuit. I will post anyway just in case it is of any help to you. Here is a little circuit that illustrates how this…
Parents
  • dougw
    0 dougw over 11 years ago

    With a normal DC motor its current will increase as it is loaded and slows down.

    So you could use a current sensor to trigger at shutoff.

    An over current breaker or fuse or even a PTC fuse might work, but these may not be precise enough or fast enough for many applications.

    A stepper motor is somewhat similar if the steps are at high enough frequency, where the armature never stops rotating, (usually above 300 Hz) but the pulsed nature of the voltage and current make measurement a bit more difficult.

    One way to detect a stepper load is to determine if the motor "slips". It should move a precise angle for every step, if it starts to "miss" steps it is slipping. This could be monitored by rotary encoder pulses which get compared to drive signal pulses.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to dougw

    I'm relatively new to the electronics scene, so what I shold do is measure the current draw of the motor and determine what it rises to under the load I want it to stop at? After I accomplish this, how do I use the sensor to trigger the shutoff? Would I use some sort of microcontroller? Thank you and sorry for my illiteracy in electronics.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 11 years ago in reply to e14 Contributor

    A microcontroller is not needed, but detailed design depends on many factors such as how big is the motor, what voltage and current are involved, how sensitive does it need to be, etc..

    Here is an example using a couple of transistors and a relay: (the motor gets hooked up at the "LOAD" terminals)

    Low Battery Cut-off and Overload Protection Circuit. | Homemade Circuit Designs Just for You

    Note R1 must be able to handle the full motor current and a small enough value that at full current there is only .7 volts across it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • dougw
    0 dougw over 11 years ago in reply to e14 Contributor

    A microcontroller is not needed, but detailed design depends on many factors such as how big is the motor, what voltage and current are involved, how sensitive does it need to be, etc..

    Here is an example using a couple of transistors and a relay: (the motor gets hooked up at the "LOAD" terminals)

    Low Battery Cut-off and Overload Protection Circuit. | Homemade Circuit Designs Just for You

    Note R1 must be able to handle the full motor current and a small enough value that at full current there is only .7 volts across it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer