Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum 24V to 1.8V for CPLD
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 5 replies
  • Answers 1 answer
  • Subscribers 502 subscribers
  • Views 848 views
  • Users 0 members are here
  • max
  • cpld
  • power
  • max_v_cpld
  • powering
Related

24V to 1.8V for CPLD

oldmanraskers
oldmanraskers over 11 years ago

Hi,

I am looking for ideas how to use an existing 24VDC power supply to power an Altera CPLD with a core voltage of 1.8V and IO Voltage of 2.5V - I'm thinking of something like a buck converter that feeds into a power conversion IC. Does anyone have examples, or suggestions on the best route to go?

Regards, oldmanraskers.

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    0 michaelkellett over 11 years ago

    Are you sure you can't use 3.3V for the IO - it will make interfacing to other stuff a whole lot easier -  the ULN...... driver chip we talked about before won't be driven properly by 2.5V.

     

    The way I would do this is to use switching regulator for the 24 -> 3.3 (prejudice showing there re. 3.3 or 2.5 image)

    Then use a linear regulator for the 3.3V -> 1.8V conversion.

    You need to check the current drain but I'm going to assume 100mA max at each voltage so your 24 -> 3.3V converter must be able to supply 200mA.

    Consider LM5008 for the switcher - not the cheapest but easy to use, adjustable output, can cope with up to 90V input, about 85% efficiency at 24V in and 200mA out.

    There are loads of other parts you could use  - some nice cheap ones from Vishay but limited max voltage, all sorts of nice and fancy ones from Linear Technology (but probably in hard to solder packages).

     

    Just search Farnell for a low drop linear regulator that you fancy - probably best to go for SO8 or SOT223 package to cope with power dissipation. there are parts with fixed 1.8V output readily available. TLV1117-18CDCYR  from TI is dirt cheap and OK for 3.3V as the higher supply - if you want the regulator to work with 2.5V input you'll need to use a more expensive part.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 11 years ago

    Are you sure you can't use 3.3V for the IO - it will make interfacing to other stuff a whole lot easier -  the ULN...... driver chip we talked about before won't be driven properly by 2.5V.

     

    The way I would do this is to use switching regulator for the 24 -> 3.3 (prejudice showing there re. 3.3 or 2.5 image)

    Then use a linear regulator for the 3.3V -> 1.8V conversion.

    You need to check the current drain but I'm going to assume 100mA max at each voltage so your 24 -> 3.3V converter must be able to supply 200mA.

    Consider LM5008 for the switcher - not the cheapest but easy to use, adjustable output, can cope with up to 90V input, about 85% efficiency at 24V in and 200mA out.

    There are loads of other parts you could use  - some nice cheap ones from Vishay but limited max voltage, all sorts of nice and fancy ones from Linear Technology (but probably in hard to solder packages).

     

    Just search Farnell for a low drop linear regulator that you fancy - probably best to go for SO8 or SOT223 package to cope with power dissipation. there are parts with fixed 1.8V output readily available. TLV1117-18CDCYR  from TI is dirt cheap and OK for 3.3V as the higher supply - if you want the regulator to work with 2.5V input you'll need to use a more expensive part.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • oldmanraskers
    0 oldmanraskers over 11 years ago in reply to michaelkellett

    I had previously seen a linear regulator that did dual outputs at 1.8V and 2.5V which is why I was going down that route... but  it sounds like 3.3V is the more useful option. Thanks Michael.