Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum How to use Xplained board with SAMA5D36 Microncrontroller (without OS on the board)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 502 subscribers
  • Views 403 views
  • Users 0 members are here
Related

How to use Xplained board with SAMA5D36 Microncrontroller (without OS on the board)

e14 Contributor
e14 Contributor over 11 years ago

Hello,

 

I am using Xplained board from Atmel with SAMA5d36 microcontroller. This board is preloaded with Linux. But I do not require linux for my application. In that case how to use this board using IAR workbench and SAMA. Can anybody help?

 

Kalpana

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 11 years ago +1
    You may want to look at Free RTOS Cortex-A5 demonstrated on a SAMA5D4 embedded Microprocessor from Atmel for ideas of using the bare hardware. Clem
Parents
  • shabaz
    0 shabaz over 11 years ago

    You may be better off with a different board if you don't require an OS on board.

    With this board, you're paying for features you cannot make use of (easily and simultaneously) if you don't run an OS. For example the memory controller, GigEth, USB..

    Although it is possible to use your own code, to use these features effectively (and together), then it's easier with an OS, and possibly near-impossible to

    practically manage code that handles multiple complex pieces of functionality without an OS (and multiple complex pieces of functionality is what the creators of the Cortex-A intended it to run).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 11 years ago

    You may be better off with a different board if you don't require an OS on board.

    With this board, you're paying for features you cannot make use of (easily and simultaneously) if you don't run an OS. For example the memory controller, GigEth, USB..

    Although it is possible to use your own code, to use these features effectively (and together), then it's easier with an OS, and possibly near-impossible to

    practically manage code that handles multiple complex pieces of functionality without an OS (and multiple complex pieces of functionality is what the creators of the Cortex-A intended it to run).