Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Choosing a Microcontroller Brand
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 47 replies
  • Answers 2 answers
  • Subscribers 507 subscribers
  • Views 7017 views
  • Users 0 members are here
Related

Choosing a Microcontroller Brand

screamingtiger
screamingtiger over 11 years ago


I understand that choosing a specific microcrontroller/processor/SOC depends on the requirements and what I am doing etc..

 

I've started a couple discussions but this one is at a critical time, I just used up my last 2 ardunio minis so I need to order a new stash.   I am considering moving away from them and to something more advanced, even if it is just using AVRs directly.

 

This question however is more about choosing a general brand of micro controllers.  In my opinion, for me, I don't have time to learn all of them.  I don't have time or $ to invest in IDEs for different platforms nor do I want a slew of them installed on my PC.

 

So help clear my ignorance here.

 

I am looking AVR, they have a wide range of products.  So does ARM.

 

If I were to say "I only want to use ARM" would I benefit from the following:

-A wide range of products from low power consumption (<100mA) all the way up to full multi core processors ( I can build small embedded projects and then go bigger if needed without having to switch brands)

 

-If I learn the assembler for one ARM product, moving to another ARM product will not result in as steep of a learning curve as the register names, instruction pnuemonics  and paradigm will be similar (subsets).

 

I could as the same question about sticking with AMTEL or PIC (microchip)

 

Does it make sense what I am trying to do?  I just want to cut down the cross system learning curves and stick with a specific set of chips that are very similar in terms of programming.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 11 years ago in reply to screamingtiger +4
    I really like the ST Nucleo boards - programmer/debugger built in, dead cheap (£7.67 for CortexM4) and quite small. MK
  • DAB
    DAB over 11 years ago +4 verified
    Hi Joey, I appear to be late to the post. I just recently purchased a couple of the Cypress Semi PSOC 4 boards. One I intend to install in my CNC mill and the others for new projects. I chose Cypress because…
  • johnbeetem
    johnbeetem over 11 years ago +2
    There are so many different ARM microcontrollers that it's hard to know what to do. In general, the core itself is pretty much the same so your real question is what on-chip peripherals do you need. Most…
Parents
  • michaelkellett
    0 michaelkellett over 11 years ago

    Inevitably we all bring our own prejudices so apologies for mine in advance, please you can take what you can from it.

     

    I design micro based systems for a living and almost always end up using an ST ARM based micro controller.  I used to use AVRs and Silabs 8051 based parts but the ARMs have left them both way behind except for one or two very special applications.

     

    I use the Keil software tool set (fully paid for version which is >£5k) but you can use it for free with up to 32k code size. Several of my customers use the free version. You can buy a basic debugger/programmer from ST for about £18 or a knockoff of the Keil Ulink for the same money or the real thing for about £200. (Or a really nice Lauterbach debugger for about £2k). Several of the ST dev boards have a built in ST link which gives you programming and debugging.

     

    If you don't like the Keil tools there are GCC based options, some of which are supported by ST. The nice thing about the ST range of ARM processors is that it's huge, they are cheap with cheap dev tools and wide acceptance and use (which makes it easier to get community based help.)

     

    Having said all that about ST, I think (but don't know because I haven't used them) that TI and Freescale both have very comprehensive offerings of parts and free dev tools.

     

    NXP have some nice hardware but the free dev tools are too Mbed based for my liking (this might be wrong - check if important - I have used NXP chips but with the Keil tools.)

     

    You asked in your original question which 'brand' and this is important - ARM is just the core (as others have mentioned) but once you pick a chip manufacturer (ST, Freescale, TI, whoever) you get to know the peripherals and the way the support libraries work etc and this always makes you inclined to stick with another part from the same source.

     

    If you use generic software tools (Keil, IAR, GCC (with or without commercial add ons)) it's easier to swap chip vendors if you need to.

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 11 years ago

    Inevitably we all bring our own prejudices so apologies for mine in advance, please you can take what you can from it.

     

    I design micro based systems for a living and almost always end up using an ST ARM based micro controller.  I used to use AVRs and Silabs 8051 based parts but the ARMs have left them both way behind except for one or two very special applications.

     

    I use the Keil software tool set (fully paid for version which is >£5k) but you can use it for free with up to 32k code size. Several of my customers use the free version. You can buy a basic debugger/programmer from ST for about £18 or a knockoff of the Keil Ulink for the same money or the real thing for about £200. (Or a really nice Lauterbach debugger for about £2k). Several of the ST dev boards have a built in ST link which gives you programming and debugging.

     

    If you don't like the Keil tools there are GCC based options, some of which are supported by ST. The nice thing about the ST range of ARM processors is that it's huge, they are cheap with cheap dev tools and wide acceptance and use (which makes it easier to get community based help.)

     

    Having said all that about ST, I think (but don't know because I haven't used them) that TI and Freescale both have very comprehensive offerings of parts and free dev tools.

     

    NXP have some nice hardware but the free dev tools are too Mbed based for my liking (this might be wrong - check if important - I have used NXP chips but with the Keil tools.)

     

    You asked in your original question which 'brand' and this is important - ARM is just the core (as others have mentioned) but once you pick a chip manufacturer (ST, Freescale, TI, whoever) you get to know the peripherals and the way the support libraries work etc and this always makes you inclined to stick with another part from the same source.

     

    If you use generic software tools (Keil, IAR, GCC (with or without commercial add ons)) it's easier to swap chip vendors if you need to.

     

    MK