Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Choosing a Microcontroller Brand
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 47 replies
  • Answers 2 answers
  • Subscribers 507 subscribers
  • Views 7054 views
  • Users 0 members are here
Related

Choosing a Microcontroller Brand

screamingtiger
screamingtiger over 11 years ago


I understand that choosing a specific microcrontroller/processor/SOC depends on the requirements and what I am doing etc..

 

I've started a couple discussions but this one is at a critical time, I just used up my last 2 ardunio minis so I need to order a new stash.   I am considering moving away from them and to something more advanced, even if it is just using AVRs directly.

 

This question however is more about choosing a general brand of micro controllers.  In my opinion, for me, I don't have time to learn all of them.  I don't have time or $ to invest in IDEs for different platforms nor do I want a slew of them installed on my PC.

 

So help clear my ignorance here.

 

I am looking AVR, they have a wide range of products.  So does ARM.

 

If I were to say "I only want to use ARM" would I benefit from the following:

-A wide range of products from low power consumption (<100mA) all the way up to full multi core processors ( I can build small embedded projects and then go bigger if needed without having to switch brands)

 

-If I learn the assembler for one ARM product, moving to another ARM product will not result in as steep of a learning curve as the register names, instruction pnuemonics  and paradigm will be similar (subsets).

 

I could as the same question about sticking with AMTEL or PIC (microchip)

 

Does it make sense what I am trying to do?  I just want to cut down the cross system learning curves and stick with a specific set of chips that are very similar in terms of programming.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 11 years ago in reply to screamingtiger +4
    I really like the ST Nucleo boards - programmer/debugger built in, dead cheap (£7.67 for CortexM4) and quite small. MK
  • DAB
    DAB over 11 years ago +4 verified
    Hi Joey, I appear to be late to the post. I just recently purchased a couple of the Cypress Semi PSOC 4 boards. One I intend to install in my CNC mill and the others for new projects. I chose Cypress because…
  • johnbeetem
    johnbeetem over 11 years ago +2
    There are so many different ARM microcontrollers that it's hard to know what to do. In general, the core itself is pretty much the same so your real question is what on-chip peripherals do you need. Most…
Parents
  • screamingtiger
    0 screamingtiger over 11 years ago

    This should not be about "which on is better",  I am ok with PIC, AVR, or ARM.  I am just wanting to pick on set, and stick with them.  I do not wish to continue with Arduino because I feel it misleads me and after a while short of getting start, it actually promotes ignorance.  This is like Visual Basic, while it is useful you are losing so much and end up being ignorant of the things that matter in the end.

     

    I dealt with a Pic32 recently and it has its own personality, and it has some quirks with I2C.  I resolved it and learned but iv I move to ARM, I may have to relearn things and also solve new problems.  I want to avoid this overhead and become proficient, even at the assembly level, one of set of chips.  I want to have a range to pick from, and as long as there is a big enough chip to work with OR a breakout board, I can live with it.  If all they sell is a small SMD chip I may not be able to use it, that would defeat the purpose.

     

    I am really leaning towards ARM but I like how PIC and AVR sell DIP versions of the chips where I can use ZIF sockets.  NOt the smallest but easy to work with!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • crjeder
    0 crjeder over 11 years ago in reply to screamingtiger

    True. In the ARM corner your choices are limited for DIP cases. But there is at least one from NXP

     

    LPC1114FN28/102,12 - NXP - 32BIT MCU IC, CORTEX-M0, 50MHZ, DIP-28 | Deutschland

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 11 years ago in reply to crjeder

    crjeder wrote:

     

    True. In the ARM corner your choices are limited for DIP cases. But there is at least one from NXP

     

    LPC1114FN28/102,12 - NXP - 32BIT MCU IC, CORTEX-M0, 50MHZ, DIP-28 | Deutschland

    NXP also has a small ARM Cortex-M0+ in an 8-pin DIP: http://www.nxp.com/products/microcontrollers/product_series/lpc800/LPC810M021FN8.html

    It has SPI, I2C, and USARTs.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • johnbeetem
    0 johnbeetem over 11 years ago in reply to crjeder

    crjeder wrote:

     

    True. In the ARM corner your choices are limited for DIP cases. But there is at least one from NXP

     

    LPC1114FN28/102,12 - NXP - 32BIT MCU IC, CORTEX-M0, 50MHZ, DIP-28 | Deutschland

    NXP also has a small ARM Cortex-M0+ in an 8-pin DIP: http://www.nxp.com/products/microcontrollers/product_series/lpc800/LPC810M021FN8.html

    It has SPI, I2C, and USARTs.