Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum ARM Keil MDK is free (sort-of)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 35 replies
  • Subscribers 502 subscribers
  • Views 21662 views
  • Users 0 members are here
  • mdkarm
  • keil
  • mdk
Related

ARM Keil MDK is free (sort-of)

shabaz
shabaz over 4 years ago

For ages, the Keil development environment/compiler which they call MDK (Microcontroller Development Kit) has been a chargeable product, extremely unaffordable for home use : (

It's really annoying when microcontroller manufacturers only supply sample code using Keil. It's not always easy to port the project files to Eclipse, often it's hard and a lot of work!

For curiosity I re-logged onto the Keil website today, and noticed there is now a Community Edition! The announcement was in March it seems.

There doesn't seem to be a code limit, which is great. 

I just now tried to build some sample code from Dialog Semiconductor (they have cheap BLE chips but 95% of the more useful example projects are with Keil, not Eclipse, hence the interest) and it worked and I was able to download to the target eval board, which has an integrated J-Link, so that works too. I'm still learning how to use Keil, it's new to me.

image

Keil has a pack system which is quite neat.. I've only installed the Dialog specific pack so far:

image

Anyway, I just thought I'd mentioned that the community edition was available, in case anyone else is interested in trying it too.

  • Sign in to reply
  • Cancel

Top Replies

  • scottiebabe
    scottiebabe over 4 years ago +2
    This is great news! That is one of my biggest complaints about the Pico, trying to setup the c development environment is way too complicated for a causal complier user.... I like one button installs,…
  • WestfW
    WestfW over 4 years ago in reply to scottiebabe +2
    > When you use the ardunio framework somewhere there is a trigger to have the rp2040 reset into bootloader mode (I'm not sure how its done) Arduino uses a hack where setting the usb/serial bitrate to…
  • Fred27
    Fred27 over 4 years ago +2
    I've only ever used Keil when exploring the Cortex M0 and M3 soft processors on Xilinx FPGAs. Keil was the only IDE supported and was way to expensive to consider beyond experimenting using the free trial…
Parents
  • KennyMillar
    KennyMillar over 3 years ago

    Windows platform only is a deal breaker for me :-(

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • KennyMillar
    KennyMillar over 3 years ago

    Windows platform only is a deal breaker for me :-(

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • michaelkellett
    michaelkellett over 3 years ago in reply to KennyMillar

    I start from the other end,

    not running the Keil tools is why I can't use Linux and have to stick with at least some Windows.

    Slight smile

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • KennyMillar
    KennyMillar over 3 years ago in reply to michaelkellett

    That made my day!

    I had a recent product requirment for a client. I evaluated what they needed, and decided an STM32F7xx would a good fit for them. I'd used the STM32 (although embedded into an AP8084 Audio processor) before, along with MDK, but my licence expired a year or so back.

    Since then I've been doing more and more on macOS and was really pleased to see how well the CUBE IDE ran on my mac. It covered all my needs and so I'm using that for now. 

    Unfortunately there's little to no tools available for my FPGA work on macOS - so I still have both PC and Mac on the desk.