Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum What open source architecture design tool do you recommend?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 23 replies
  • Answers 1 answer
  • Subscribers 503 subscribers
  • Views 8701 views
  • Users 0 members are here
Related

What open source architecture design tool do you recommend?

Jairo
Jairo over 4 years ago

Hi, could you recommend me an open source to design my embedded system project architecture?, actually I use diagrams.net to create my block diagrams but maybe there is a more professional tool, thanks

  • Sign in to reply
  • Cancel

Top Replies

  • phoenixcomm
    phoenixcomm over 4 years ago in reply to shabaz +2 suggested
    /members/shabaz /members/scottiebabe I think you should both look at Flameshot (Linux) which works like Snagit (MS). see look at the Linux alternative.
  • phoenixcomm
    phoenixcomm over 4 years ago in reply to shabaz +2
    my lord, I used to use two UltraSPARC 2 for my ISP one was the web server the other was the mail server, and I used a SPARC lunchbox to run Tic and Toc for my NTPd server. Take a look at the clock on top…
  • dougw
    dougw over 4 years ago +1
    Diagrams.net looks pretty reasonable. I just use Libre Office presentation tools. I try to keep the block diagrams simple and high level.
Parents
  • shabaz
    0 shabaz over 4 years ago

    Seems a bit spammy, considering that you mentioned a non-open-source tool. Why does it need to be an open source tool? There are plenty of more professional tools than the non-open-source one that you mentioned, but they are not open source either.

    What's wrong with PowerPoint, or the free equivalents like Libre Office?

    If you want a proper professional tool as actually used in industry, I can suggest some but they are not open source.
    If it is work related, then there may be an application the organisation wishes you to use, or, sometimes they won't care whatever app you use, since the output doesn't directly drive automation in the project management (i.e. it's not directly coupled). If you want others to also be able to work with the design, then you probably want to stick to an app that others have access to. I wouldn't trust the cloud version of that app, and I can't see I'd want anything from that app that you refer to, when PowerPoint will work for me if I'm not being mandated to use any other app.

    • Cancel
    • Vote Up -1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 4 years ago

    Seems a bit spammy, considering that you mentioned a non-open-source tool. Why does it need to be an open source tool? There are plenty of more professional tools than the non-open-source one that you mentioned, but they are not open source either.

    What's wrong with PowerPoint, or the free equivalents like Libre Office?

    If you want a proper professional tool as actually used in industry, I can suggest some but they are not open source.
    If it is work related, then there may be an application the organisation wishes you to use, or, sometimes they won't care whatever app you use, since the output doesn't directly drive automation in the project management (i.e. it's not directly coupled). If you want others to also be able to work with the design, then you probably want to stick to an app that others have access to. I wouldn't trust the cloud version of that app, and I can't see I'd want anything from that app that you refer to, when PowerPoint will work for me if I'm not being mandated to use any other app.

    • Cancel
    • Vote Up -1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • phoenixcomm
    0 phoenixcomm over 4 years ago in reply to shabaz

    You do realize that LibreOffice supports MS extensions.