Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Bluetooth stereo module v3.0 make the sound like "Bluetooth device is connected"
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 502 subscribers
  • Views 2206 views
  • Users 0 members are here
  • bluetooth
  • embedded hardware
  • stm32f4discovery
  • bluetooth low energy (ble)
  • arduino
Related

Bluetooth stereo module v3.0 make the sound like "Bluetooth device is connected"

mqureshi
mqureshi over 3 years ago

I want to make a project in which

  1. I want to play music form smart phone inside the robo car.
  2. Operate the robotic car(Motors) from mobile application.

Challange: -

  1. Is there is any Bluetooth module which can communicate with robot car and play music at the same time.
  2. I had use two separate module HC05 for controlling the motor and Bluetooth V3.0 stereo module for playing the music. When the power is on " V3.0 stereo module" make sound like " Bluetooth device is connected or Bluetooth device is ready to pair.

Can this this voice can be removed or is there is module readily available where we can remove this voice and communicate with the microcontroller at the same time?

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    shabaz over 3 years ago

    Hi,

    This doesn't sound like a very top-priority key feature for your project. I'd suggest, build your project, make it do the main things (music/motors) and once you've done that, you will be able to just extend your project to mute out the audio, by using the same system that you're using to control the motors, prior to enabling the music channel.

    There are many other solutions, but you'll gain the experience by just trying, In this case, I think you can extend and modify once you have the rest working. This approach doesn't always work, but in this case it likely will.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mqureshi
    mqureshi over 3 years ago in reply to shabaz

    Hi Shabaz, 

    Thanks for the reply

    My target is that to remove the annoying voice when the power is on. 

    How can we remove it? 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 3 years ago in reply to mqureshi

    You'll have to look into modifying the firmware. It used to be more often seen for CSR BlueCore-based devices, but that scene is now relatively quiet and the tools unsupported. You'll need to do your own research as it is very much chipset-specific.

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Gough Lui
    Gough Lui over 3 years ago in reply to mqureshi

    You'll have to look into modifying the firmware. It used to be more often seen for CSR BlueCore-based devices, but that scene is now relatively quiet and the tools unsupported. You'll need to do your own research as it is very much chipset-specific.

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • mqureshi
    mqureshi over 3 years ago in reply to Gough Lui

    Thanks Lui. 

    Thanks for the suggestion. I will try if I will stuck then I will ask.