Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Bluetooth stereo module v3.0 make the sound like "Bluetooth device is connected"
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 502 subscribers
  • Views 2201 views
  • Users 0 members are here
  • bluetooth
  • embedded hardware
  • stm32f4discovery
  • bluetooth low energy (ble)
  • arduino
Related

Bluetooth stereo module v3.0 make the sound like "Bluetooth device is connected"

mqureshi
mqureshi over 3 years ago

I want to make a project in which

  1. I want to play music form smart phone inside the robo car.
  2. Operate the robotic car(Motors) from mobile application.

Challange: -

  1. Is there is any Bluetooth module which can communicate with robot car and play music at the same time.
  2. I had use two separate module HC05 for controlling the motor and Bluetooth V3.0 stereo module for playing the music. When the power is on " V3.0 stereo module" make sound like " Bluetooth device is connected or Bluetooth device is ready to pair.

Can this this voice can be removed or is there is module readily available where we can remove this voice and communicate with the microcontroller at the same time?

  • Sign in to reply
  • Cancel
Parents
  • dougw
    dougw over 3 years ago

    Does the music need to come through Bluetooth? Could you use an onboard MP3 player instead?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 3 years ago

    Does the music need to come through Bluetooth? Could you use an onboard MP3 player instead?