Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum PSoC4 SPI LoRa PROBLEM
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 502 subscribers
  • Views 2137 views
  • Users 0 members are here
  • spi interface
  • spi
  • embedded
  • microcontroller
  • psoc
Related

PSoC4 SPI LoRa PROBLEM

MKocaman
MKocaman over 3 years ago

Hello to everyone,
I'm new to PSoC and trying to learn. I have the PSoC4 CY8CKIT-041 kit. I'm struggling to run the LoRa module by communicating with SPI. The LoRa module is a module that I know well and that I run on processors such as STM32, Renesas. But I'm having trouble with PSoC, I'm stuck especially on SPI. I have attached pictures of SPI TX and RX functions and added the project separately. You can check. Can you help me for sending and receiving commands in SPI? Can you create the correct command functions for me? Thank you from now.

image

image

image

image

image

lesson1.zip

  • Sign in to reply
  • Cancel

Top Replies

  • KennyMillar
    KennyMillar over 3 years ago +2
    Hi MKocaman Wow - PSoC 4 - that takes me back a wee bit! So a few things first that I'll check with you. In the SPI_Tx function you are resetting and setting LoRa_RESET - are you shure that's right…
  • KennyMillar
    KennyMillar over 3 years ago in reply to MKocaman +2
    Can you tell me which LoRa module you are using? Do you have a link to a datasheet?
  • KennyMillar
    KennyMillar over 3 years ago +1
    Hi MKocaman So in your function Modul_Reset() in LoRa.c you set the reset and NSS pins high, then delay, then set the RESET pin low again. This leaves the NSS pin high. I don;t see it being referenced…
Parents
  • KennyMillar
    KennyMillar over 3 years ago

    Hi MKocaman 

    Wow - PSoC 4 - that takes me back a wee bit!

    So a few things first that I'll check with you.

    In the SPI_Tx function you are resetting and setting LoRa_RESET - are you shure that's right? (I don't have the LoRa module to check with).

    Also, I see there is a pin called LoRa_NSS - are you sure you are handling that correctly? Shouldn't you be driving that low for SPI transactions?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • KennyMillar
    KennyMillar over 3 years ago

    Hi MKocaman 

    Wow - PSoC 4 - that takes me back a wee bit!

    So a few things first that I'll check with you.

    In the SPI_Tx function you are resetting and setting LoRa_RESET - are you shure that's right? (I don't have the LoRa module to check with).

    Also, I see there is a pin called LoRa_NSS - are you sure you are handling that correctly? Shouldn't you be driving that low for SPI transactions?