Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum variables values not showing equal
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 501 subscribers
  • Views 3505 views
  • Users 0 members are here
  • embedded
Related

variables values not showing equal

Dnyaneshwar07
Dnyaneshwar07 over 3 years ago

Hello everyone,

                       i am using renesas rx231 series microcontroller and E2 studio ide for code development,

                         i have written one small code in which i have taken one signed int whoes value is -3871,and another variable which is also same signed int with value of 61665 which its 2's compliment value  -3871and another same variable i have taken signed int with hex value of -3871 which is 0xF0E1 ,with this i have written one if else statement but it is not working/not showing the same value.

signed int i = -3871;
signed int j = 0xf0e1;
signed int k = 61165;

_Bool m;

void main(void)
{

while(1)
{
R_Config_WDT_Restart();

if(j == k)
{
m = 1;
}
else if(j == i)
{
m = 1;
}
else if(k == i)
{
m = 1;
}
else
{
m = 0;
}
}

}

value of m remains 0 always.why this is happening??

please any can explain this?

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 3 years ago +2
    You would do yourself a favour by using more modern C coding practice: add these includes to the start of every module: #include <stdint.h> #include <stdbool.h> declare 16 bit integers like this…
  • michaelkellett
    michaelkellett over 3 years ago in reply to phoenixcomm +2
    Arguments about C coding standards are as never-ending as those about religion. However, your suggestion re. Pascal is not rational - almost all micro-controllers are supported by a choice of C compilers…
  • javagoza
    javagoza over 3 years ago +1
    Are you sure that the data type int is 2 bytes and not 4 bytes? You are using only 2 bytes (16 bits) to represent an int value. It is more common to use 4 bytes (32 bits). I don't know the compiler you…
Parents
  • shabaz
    shabaz over 3 years ago

    In situations like this, there are lots of things you can do to better understand what the compiler is doing. One way is to examine the assembler listing file (enable it in your project settings in whatever IDE you're using). Another way is to manually observe from your debugger tool's memory or variable dump. Yet another way is to write yourself a print function which will dump memory (you can cast the pointer to your variables to say char type) and then sequentially dump out each memory location for your variables so you can inspect them. Also, get used to examining the settings in the IDE for the project, because some compilers can be configured for different data sizes. Also, check the optimisation settings, just in case if you're not actually using a variable (you are not using the variable m at all, you are only setting it) the compiler may remove it completely, i.e. optimise it out, because you don't specify how you checked m. Also, you could consider making use of stdint.h (uint8_t etc).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 3 years ago

    In situations like this, there are lots of things you can do to better understand what the compiler is doing. One way is to examine the assembler listing file (enable it in your project settings in whatever IDE you're using). Another way is to manually observe from your debugger tool's memory or variable dump. Yet another way is to write yourself a print function which will dump memory (you can cast the pointer to your variables to say char type) and then sequentially dump out each memory location for your variables so you can inspect them. Also, get used to examining the settings in the IDE for the project, because some compilers can be configured for different data sizes. Also, check the optimisation settings, just in case if you're not actually using a variable (you are not using the variable m at all, you are only setting it) the compiler may remove it completely, i.e. optimise it out, because you don't specify how you checked m. Also, you could consider making use of stdint.h (uint8_t etc).