Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum OO Digital Pin class: single class or separate in and out classes
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 37 replies
  • Subscribers 501 subscribers
  • Views 6621 views
  • Users 0 members are here
Related

OO Digital Pin class: single class or separate in and out classes

Jan Cumps
Jan Cumps over 3 years ago

I'm experimenting with light-weight C++ for microcontrollers. Looking for your opinion for class(es) that represent GPIO pin behaviour

An output pin can

  • accept a value and set it
  • return the value it is set to
  • maybe go high-z

An input can:

  • return the value at its input

I may represent this

  • very simple as a single class.
    Getting the value would perform the "return" action above. The class would decide if it returns output state or input state internally
    Setting would only succeed if the pin is an output pin, else either throw an exception or silently ignore.
    Switching between the two would be simple
  • as separate classes
    out type pin would set the output as indicated, and return the output state if asked
    in type pin would return the value at its input. It would not provide setters.
    Switching between two modes would mean discarding the original object and creating one of the other kind.
    (should both classes inherit from a common parent that defines the actual pin?)

How would you solve this, as OO designer / abstractor that loves simplicity?

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 3 years ago in reply to michaelkellett +3
    The compiler was way better than I thought... I gave it a shot with the GNU compiler for ARM, using the Pi Pico SDK. I created a simple class: Then that class is used in the main() function. The…
  • ggabe
    ggabe over 3 years ago +2
    Take a look at WiringPi, as an example how the single class API can be structured: http://wiringpi.com/reference/ I like how it can abstract MCU GPIO and IO expanders under the same API. if you need…
  • Andrew J
    Andrew J over 3 years ago +2
    On the basis of your points above, what you are essentially describing is a variable: you can set a value and you can read a value. I don't think that would benefit from being encapsulated by a class and…
Parents
  • Jan Cumps
    Jan Cumps over 3 years ago

    I've tried it with a single class, as suggested by shabaz and ggabe .

    You'd use it like this:

    #include <IO.h>
    
    io::IO led(GPIO_PORT_H_PIN_2);  // initialise the output pin for the LED.
    io::IO button(GPIO_PORT_2_PIN_7); // push button
    
    int main(void) {
    
    	int i;
        while(1) {
        	led = button;
    
        	// silly wait
        	for (i = 0; i < 100000; i++) {nop();};
        }
    

    Header (API):

    namespace io {
    
    typedef gpio_port_pin_t pin_t;
    typedef gpio_dir_t dir_t;
    
    class IO {
    public:
    	IO(pin_t pin);
    	virtual ~IO();
        IO &operator!= (IO &rhs); // take over the inverted state of rhs
    	IO &operator= (IO &rhs); // take over the  state of rhs
    	IO &operator= (bool high);
    	operator bool() const;
    	void setDirection(dir_t dir);
    protected:
    	pin_t pin;
    private:
    };

    The button behaves like a button, the led as a led. 
    For the programmer/user, they act as variables.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Jan Cumps
    Jan Cumps over 3 years ago

    I've tried it with a single class, as suggested by shabaz and ggabe .

    You'd use it like this:

    #include <IO.h>
    
    io::IO led(GPIO_PORT_H_PIN_2);  // initialise the output pin for the LED.
    io::IO button(GPIO_PORT_2_PIN_7); // push button
    
    int main(void) {
    
    	int i;
        while(1) {
        	led = button;
    
        	// silly wait
        	for (i = 0; i < 100000; i++) {nop();};
        }
    

    Header (API):

    namespace io {
    
    typedef gpio_port_pin_t pin_t;
    typedef gpio_dir_t dir_t;
    
    class IO {
    public:
    	IO(pin_t pin);
    	virtual ~IO();
        IO &operator!= (IO &rhs); // take over the inverted state of rhs
    	IO &operator= (IO &rhs); // take over the  state of rhs
    	IO &operator= (bool high);
    	operator bool() const;
    	void setDirection(dir_t dir);
    protected:
    	pin_t pin;
    private:
    };

    The button behaves like a button, the led as a led. 
    For the programmer/user, they act as variables.