Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Measuring liquid level of a sealed container
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 18 replies
  • Subscribers 497 subscribers
  • Views 3957 views
  • Users 0 members are here
Related

Measuring liquid level of a sealed container

Hasanga
Hasanga over 2 years ago

I need to measure liquid level inside a sealed container there can't be placed any sensors inside it. This is a shock absorber in a very powerful machine. So in operation the pressure and temperature will be high and flowing speed of liquid is also high . 

   1. Container is steel cylinder, height 1 meter, diameter 8 inches,          wall thickness 3 mm. it      can be tilted horizontal to 60 degrees         in vertical. But can't be            moved. It contains a nother hollow       steel cylinder.

         a. This small cylinder is same height, diameter 5 inches. And             have a orifice of 5 cm on its wall so liquid can move in and out            from this cylinder to outer cylinder freely. 

I will be measuring liquid level before operation and during trouble shooting only. What methods can be used?

  • Sign in to reply
  • Cancel

Top Replies

  • beacon_dave
    beacon_dave over 2 years ago in reply to shabaz +3
    shabaz said: not realizing that just a few milli-litres causes enough vapor to be dangerous Tim Hunkin & Rex Garrod - teaspoon of gunpowder vs teaspoon of petrol: https://youtu.be/qyVHzJ40JqM?list…
  • dougw
    dougw over 2 years ago +1
    What is the liquid? How does the liquid get in and out of the cylinder? How accurately do you need to know the liquid level? Without knowing more about the system, your best bet is likely to somehow…
  • Fred27
    Fred27 over 2 years ago +1
    This sounds like a difficult problem - especially as any modification to the shock absorber could be very dangerous. Why do you want to measure the liquid level? What exactly is the problem you're trying…
Parents
  • rsc
    rsc over 2 years ago

    In a hydraulic cylinder, the stroke (h) of the cylinder is proportional to the volume of liquid in the cylinder = 3.14*(D1*D1/4)h

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rsc
    rsc over 2 years ago

    In a hydraulic cylinder, the stroke (h) of the cylinder is proportional to the volume of liquid in the cylinder = 3.14*(D1*D1/4)h