Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Measuring liquid level of a sealed container
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 18 replies
  • Subscribers 497 subscribers
  • Views 3967 views
  • Users 0 members are here
Related

Measuring liquid level of a sealed container

Hasanga
Hasanga over 2 years ago

I need to measure liquid level inside a sealed container there can't be placed any sensors inside it. This is a shock absorber in a very powerful machine. So in operation the pressure and temperature will be high and flowing speed of liquid is also high . 

   1. Container is steel cylinder, height 1 meter, diameter 8 inches,          wall thickness 3 mm. it      can be tilted horizontal to 60 degrees         in vertical. But can't be            moved. It contains a nother hollow       steel cylinder.

         a. This small cylinder is same height, diameter 5 inches. And             have a orifice of 5 cm on its wall so liquid can move in and out            from this cylinder to outer cylinder freely. 

I will be measuring liquid level before operation and during trouble shooting only. What methods can be used?

  • Sign in to reply
  • Cancel

Top Replies

  • beacon_dave
    beacon_dave over 2 years ago in reply to shabaz +3
    shabaz said: not realizing that just a few milli-litres causes enough vapor to be dangerous Tim Hunkin & Rex Garrod - teaspoon of gunpowder vs teaspoon of petrol: https://youtu.be/qyVHzJ40JqM?list…
  • dougw
    dougw over 2 years ago +1
    What is the liquid? How does the liquid get in and out of the cylinder? How accurately do you need to know the liquid level? Without knowing more about the system, your best bet is likely to somehow…
  • Fred27
    Fred27 over 2 years ago +1
    This sounds like a difficult problem - especially as any modification to the shock absorber could be very dangerous. Why do you want to measure the liquid level? What exactly is the problem you're trying…
Parents
  • kmikemoo
    kmikemoo over 2 years ago

    Perhaps an unconventional ultrasonic solution. I don't know if this concept will work, but...
    The cylinder with the hydraulic oil will be more dense than the cylinder without it. Set the sensor outside the second cylinder and at a level just below the oil. If the oil level falls, the ultrasonic reading should change.  Maybe it's not ultrasonics, but whacking an empty cylinder produces a different sound that whacking one filled with liquids.  Maybe it's a series of vibrational sensors.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Hasanga
    Hasanga over 2 years ago in reply to kmikemoo

    Thank you all for your time and effort for trying to help. This is just a routine check. It's like you check oil level by dip stick on car time to time or if you have not used it for a while. You just make sure it for safety. This is very crucial in this machine as if it fails many lives may be lost. So it's a safety measure.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Hasanga
    Hasanga over 2 years ago in reply to Hasanga

    I did some searching, there was a suggestion to check temperature from outside along the cylinder as liquid will quickly absorb heat energy rather than air. At the interface there will be change of temperature. Will this be a practical solution what are the challenges to it?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Fred27
    Fred27 over 2 years ago in reply to Hasanga
    Hasanga said:
    This is very crucial in this machine as if it fails many lives may be lost.

    If this is true then it really isn't compatible with asking random strangers on the internet for a solution - especially when they don't have all the background information.

    I'll be the first to say that the people replying to you here in E14 are some of the smartest and most helpful people you'll find online. However, this is not enough if you're working on something with the potential to kill.

    Speak to the manufacturer of this machine. Get someone who is qualified to devise a solution to do so. Anything else is irresponsible and perhaps even criminal.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Fred27
    Fred27 over 2 years ago in reply to Hasanga
    Hasanga said:
    This is very crucial in this machine as if it fails many lives may be lost.

    If this is true then it really isn't compatible with asking random strangers on the internet for a solution - especially when they don't have all the background information.

    I'll be the first to say that the people replying to you here in E14 are some of the smartest and most helpful people you'll find online. However, this is not enough if you're working on something with the potential to kill.

    Speak to the manufacturer of this machine. Get someone who is qualified to devise a solution to do so. Anything else is irresponsible and perhaps even criminal.