Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum LCD got dark, any idea why?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 498 subscribers
  • Views 2408 views
  • Users 0 members are here
  • charging
  • lcd displays
Related

LCD got dark, any idea why?

koudelad
koudelad over 2 years ago

Hello,

I have a universal charger for up to 4 battery packs. Over the past year, 4 displays in the device got partially dark and are readable from different angles only, not from the standard 6:00 view.

Any idea why this happened? I think it was not in direct sunshine, but guarantee (even if it did, if was in behind a strong glass and ventilated area). It was in operation for charging maybe ca 100 cycles for some battery packs and the unit is 1-2 years old. Maybe heat from the inside? (Poor thermal design? I haven't opened the unit, yet).

I hope the LCDs could get replaced, but I am afraid it will happen again.

battery charger

Thank you,

David

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 2 years ago in reply to Jan Cumps +3
    All causes should be low probability, Here is a more in depth list of some possibilities... The LCD sandwiches have this bias when built due to manufacturing tolerances, but it can be overcome by the…
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to Gough Lui +2
    Could it be related to an improper firmware/driver, that messes with the display drive waveforms? If they aren't properly balanced, LCDs can become charged. Wondering because all 4 have a similar shadow…
  • kmikemoo
    kmikemoo over 2 years ago in reply to dougw +1
    dougw Good list. Fluke displays exhibited loss of characters due to the elastomeric connector oxidizing. A little alcohol and allowing them to flex a bit usually brought them back in line. My guess…
  • Gough Lui
    Gough Lui over 2 years ago

    I've had many HD44780-based/clone displays and I've not seen this sort of thing happen just to the middle. I would suspect heat or maybe pressure on the glass sandwich, but perhaps maybe it's a problem with that particular batch or model of display ... or maybe the way they are mounted causes some "warp" or pressure to accumulate in the centre.

    Usually if it were a problem with the analog contrast voltage, then it would affect the display uniformly, rather than in the centre.

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to Gough Lui

    Could it be related to an improper firmware/driver, that messes with the display drive waveforms? If they aren't properly balanced, LCDs can become charged. Wondering because all 4 have a similar shadow pattern.

    https://www.sparkfun.com/datasheets/LCD/HD44780.pdf page 37.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • koudelad
    koudelad over 2 years ago

    Thank you for the replies,. I also haven't seen this before. I suspected heat, but I guess it wouldn't be that similar on all 4 of them. I never noticed the unit hot, but it definitely can generate some heat, since the thermal design includes a fan which is blowing air from the side.

    I will check the mechanical pressure, it is not obvious without opening. The displays are under some front panel that is fully covered by a foil (transparent over the displays) and foil keys under the displays.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 2 years ago

    As mentioned it is likely related to stress and strain on the glass. You can gently push on different areas or gently lift different areas with some tape to see the effect of pressure.

    Display contrast and angle control using bias voltage adjustment can optimize display characteristics, possibly enough to improve this situation. Some displays have a pot to adjust the bias.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to dougw
    dougw said:
    related to stress and strain on the glass

    If it was one, or some displays, yes. But here we see the exact same flaw on all four displays (lower row central characters impacted). I don't know how that can happen on all of them, gradually, in 4 years.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 2 years ago in reply to Jan Cumps

    All causes should be low probability, Here is a more in depth list of some possibilities...

    • The LCD sandwiches have this bias when built due to manufacturing tolerances, but it can be overcome by the correct electrical bias, however over time the electrical bias has drifted, exposing the manufacturing tolerance issue.
    • The LCD sandwiches are clamped in frames that apply pressure around the edges. Over time the center sections bow out a bit causing the middle areas to need a different drive bias.
    • The LCDs are mounted in the panel using screws that apply an uneven stress on the LCD and over time the LCD deforms slightly.
    • If the LCDs use an elastomeric connector on a PCB, the PCB may bow over time causing a different impedance to some signals (this is common with elastomeric connectors)
    • There is some hot component under that area in each display that is causing thermal expansion and something has fatigued enough for it to cause an issue.

    Like I said, so far only low probability ideas...

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • kmikemoo
    kmikemoo over 2 years ago in reply to dougw

    dougw Good list. Thumbsup

    Fluke displays exhibited loss of characters due to the elastomeric connector oxidizing.  A little alcohol and allowing them to flex a bit usually brought them back in line.

    My guess is it's related to heat.  The output levels listed on the front of the charger are pretty beefy.  AND... the pushbuttons are on the bottom.  Maybe there's some correlation there.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to dougw

    One of the older data sheets contains operation cautions: https://datasheet.datasheetarchive.com/originals/scans/Scans-049/DSADA001252.pdf 

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • James123
    James123 over 2 years ago

    It’s likely due to prolonged use, which is quite normal for performance degradation.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to James123

    Not when properly driven though. Degradation because of improper balanced signals usually shows after intensive use. Properly driven displays stay clear for a lifetime.