Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Bit angle modulation
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 502 subscribers
  • Views 277 views
  • Users 0 members are here
Related

Bit angle modulation

steve25
steve25 over 9 years ago

Hi all,

 

A few years ago i built an LED cube and i never stop wandering how it actually worked. So i did some research and found that bit angle modulation was one of the most important aspect of it. I couldn't really find any C code examples so i created my own. The code turns a led on and makes it more brighter. Is there a way to make the code more efficiëntly?

 

/***************************************
* PROJECT: Bit angle modulation example
* AUTHOR: Steve
* VERSION: 1.0
**************************************/


#define F_CPU 16000000UL //Define CPU speed because timing for the interrupt is important. 


#include <avr/io.h>
#include <avr/interrupt.h>
#include <math.h>


int bitResolution[8]; //Define the bit resolution for the bit angle modulation. In this case it's 8-bit.
int bitShift = 0; //Used to store a bit value.
int ledBrightness = 0; //Used to store the led brightness.
int cycleCounter = 0; //Used to count the micro controller cycles.


int main(void)
{

  ioInit();

    while (1) 
    {
  if(ledBrightness > (int)pow(2,(sizeof(bitResolution)/sizeof(int)))-1) //When the brightness value is bigger than the maximum bit value (2^8=255 (counted from zero) in this case).
  {
  ledBrightness = 0;
  }
  brightnessMask(ledBrightness); //Calling method that handles the bit mask.
  bitAngleModulation(); //Calling method that handles the bit angle modulation (BAM).
    }

}


void ioInit()
{
  TCNT1 = 0x00; //Initialize the timer value.
  TCCR1B = 0x0D; //Enable the CTC mode and prescale the clock by 1024 (clock/1024).
  TIMSK1 = 0x02; //Enable interrupt on match between OCR1A and TCNT1.
  OCR1A = 15; //After 15 cycles there is a match between OCR1A and TCNT1. A interrupt will occur.
  sei(); //Enable interrupts.

  DDRD = 0x01; //Define the output register.

}


void brightnessMask(int brightness)
{
  for(int i = (sizeof(bitResolution)/sizeof(int) - 1); i >= 0; i--) //I use a decreasing for loop. Because the bit value always counts from right to left. So we want to have the lowest value on place 1 in the array.
  {
  if(brightness - (1<<i) >= 0) //Compares if the brightness value minus the shifted value is bigger or equal as zero. If that is the case the bit should be 1. Otherwise 0.
  {
  brightness -= (1<<i); //Safe the current value
  bitResolution[i] = 1; //Write a one to a specific array place.
  }
  else
  {
  bitResolution[i] = 0; //Write a zero to a specific array place.
  }
  }
}


void bitAngleModulation()
{
  for(int i = 0; i < sizeof(bitResolution)/sizeof(int);i++) //Loop as long as the value of the bit angle modulation you defined.
  {
  bitShift = (1<<i); //Store the value of the current bit.
  for(int j = 0; j < bitShift; j++) //Loop as long as the value of the current bit. (Example: 0b0100 has a value of 4. This means that the for loop would loop 4 times)
  {
  if(bitResolution[i] == 1) //Compare if the specific array place contains a bit value of 1.
  {
  PORTD = 0x01; //Enable the output
  }
  else
  {
  PORTD = 0x00; //Disable the output
  }
  }
  }
}


ISR(TIMER1_COMPA_vect)
{
  /* Calculate how fast you want to change brightness. It is done with the following calculation: 
  Clockspeed/prescaler/OCR1A/100 = brightness change frequency. So in this case it goes as followed:
  16.000.000/1024//15/100 = 10,41 hertz. This would mean that it takes (1/10,41)*255 = 24,52 seconds to go from 0-255.
  */
  if(cycleCounter > 100)
  {
  cycleCounter=0; //Reset cycle counter
  ledBrightness++; //Increase brightness by 1.
  }

  cycleCounter++; //Increase cycle counter by 1.

}