Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum delay generation
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 504 subscribers
  • Views 2036 views
  • Users 0 members are here
Related

delay generation

mr.rohit
mr.rohit over 9 years ago

Delay generation using timer in pic18f46k22

 

I am using timer interrupt for delay generation in pic18f

when i generate  any delay using timer that time this delay is not proper which i want,it showing some difference in time.

i want knw what is the reason of that difference ?

plz help me...

thank u..

  • Sign in to reply
  • Cancel

Top Replies

  • koudelad
    koudelad over 9 years ago in reply to mr.rohit +4
    Well... A calculator is useful only after you fully understand, what it calculates. There is no information about age or function... First, trust the datasheet of PIC18F46K22 . Microchip tries to have…
  • koudelad
    koudelad over 9 years ago in reply to mr.rohit +4
    I am glad I could help. And welcome to element14 community To be honest, when I started with 16F PICs (13 years ago), I only had some book that didn't provide much explanation. Then I opened the datasheet…
  • koudelad
    koudelad over 9 years ago +3
    Hello, there are too many variables. The more details you add, the more we would be able to help you. Basically, I would focus on the following: 1) oscillator frequency and stability - this is crucial…
Parents
  • koudelad
    koudelad over 9 years ago

    Hello,

    there are too many variables. The more details you add, the more we would be able to help you.

    Basically, I would focus on the following:

    1) oscillator frequency and stability - this is crucial - are you using an integrated RC or some kind of external oscillator? (What are the conditions your design works in? e.g. variable temperature..)

    2) is your timer (and prescaler / postscaler) set correctly?

    3) do you work with the timer properly? (for example if you generate periodically an interrupt, but have poorly written ISR, it looses precision; the same if multiple interrupts occur at once or even worse, the same source of interrupt occurs multiple times, before you finish the ISR)

    4) What makes you think that you have a difference in time delay? Do you have any measurement instrument? What delays are you trying to achieve?

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • koudelad
    koudelad over 9 years ago

    Hello,

    there are too many variables. The more details you add, the more we would be able to help you.

    Basically, I would focus on the following:

    1) oscillator frequency and stability - this is crucial - are you using an integrated RC or some kind of external oscillator? (What are the conditions your design works in? e.g. variable temperature..)

    2) is your timer (and prescaler / postscaler) set correctly?

    3) do you work with the timer properly? (for example if you generate periodically an interrupt, but have poorly written ISR, it looses precision; the same if multiple interrupts occur at once or even worse, the same source of interrupt occurs multiple times, before you finish the ISR)

    4) What makes you think that you have a difference in time delay? Do you have any measurement instrument? What delays are you trying to achieve?

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Children
  • mr.rohit
    mr.rohit over 9 years ago in reply to koudelad

    i am  using DSO for time period measurement

    i want time delay in microsecond for CTMU unit in pic18f46k22

    i am using internal oscillator with PLL - 64MHz (16MHz  + 4xPLL),

     

    my timer register detail is

     

     

    T0CONbits.T0PS = 1;                 //timer0 prescalar enable    

        T0CONbits.PSA = 1;

        T0CONbits.T0PS0 = 0;

        T0CONbits.T0PS1 = 0;

        T0CONbits.T0PS2 = 0;

        T0CONbits.T08BIT = 1; //8 BIT MODE

        INTCONbits.TMR0IE = 1; //Enable TIMER0 Interrupt

        T0CONbits.TMR0ON = 1; //Now start the timer!

        T0CONbits.T0CS = 0;

        TMR0 = 254; //load count in TMR0 register