Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Does the Embedded Group Need A Better Definition?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 504 subscribers
  • Views 1819 views
  • Users 0 members are here
Related

Does the Embedded Group Need A Better Definition?

rscasny
rscasny over 9 years ago

As I've indicated to some members, part of my job at element14 (besides RoadTests, Webinars, Design Challenges) is to monitor the content in various groups to ensure we are covering topics of interest to our members or to find interesting member-content to highlight or promote (or even to find exceptional writers.)

 

I often look at the Embedded group. I'm wondering if it needs better definition. We say it is focused on "microcontrollers, programmable logic, memory, DSP and controllers." Each of these are a big area unto themselves.

 

If anyone has any thoughts on this, please offer them in the comments below.

 

Thanks.

 

Randall

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 9 years ago in reply to rscasny +5
    I'm a fan of a good explanation and few if no subgroups. I have two reasons for that: - subgroups create more confusion than solution. - blogs in subgroups don't get views, and comments are mostly from…
  • rscasny
    rscasny over 9 years ago in reply to dougw +4
    I don't disagree that the names of our groups on some level "have commercial significance." But I don't think that's our first concern. A healthy community that encourages participation and engagement…
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to rscasny +4
    Again... I was thinking also to another option, despite remain a good idea to make the name more "popular". Celebrating the new name can be a good idea to launch a series of projects focused on the use…
Parents
  • dougw
    dougw over 9 years ago

    I can't speak for others, but this category and terminology was never used where I went to school nor anyplace I ever worked. It has certainly garnered a place as a catch-all category even with big conferences using it in their name, but lay-people wouldn't have a clue to its significance and I almost never use the term embedded when discussing applications that would fall into this category. If I was publishing a blog describing an embedded application, I would typically look for a more specific group to attach it to.

    I have nothing against having it as a catch-all group category on the forum, it probably should be there, I just don't hang out in that group, even though much of what I do is embedded.

    I always assumed the Topics (groups) were chosen for their commercial significance to element14 - I don't hang out in any of them - I just read all the blog posts and discussions  from all groups.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 9 years ago in reply to dougw

    I agree with Douglas.

     

    Embedded was a term used in the 1980's but it is really meaningless with today's options.

     

    I would go with something like Makerspace Electronics to better define the focus on using electronics of all types for builds.

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 9 years ago in reply to DAB

    Embedded computers or computing used to mean computers embedded into a system to such an extent that the computer was either not apparent or not important to the user of the system:

     

    see  Wiki: https://en.wikipedia.org/wiki/Embedded_system

    An embedded system is a computer system with a dedicated function within a larger mechanical or electrical system, often with real-time computing constraints.[1][2] It is embedded as part of a complete device often including hardware and mechanical parts. Embedded systems control many devices in common use today.[3] Ninety-eight percent of all microprocessors are manufactured as components of embedded systems.[4]

     

    The term is more broadly used now but I think it is still relevant, I interpret "Embedded" as a shortening of "Embedded Computing", but perhaps that's not as universal as I thought.

     

    I don't feel that Makerspace Electronics is the same thing - the "Maker" thing has, to me at least, more social/political overtones and is less of a technology definition.

     

    Finally, I'm with Douglas on this, I look at stuff that seems interesting - people often post in the wrong group anyway.

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 9 years ago in reply to DAB

    DAB wrote:

     

    Embedded was a term used in the 1980's but it is really meaningless with today's options.

    I guess its dependant on the types of companies you've been working in. For me, "Embedded" is a term that has always been used extensively in the places I have worked and still is. For example, our software teams are usually split into the "Applications" team which are responsible for writing UI applications which run on standard PC's, and the "Embedded Software" teams who deal with all the OS and software running on "non desktop" platforms as well as the DSP code running on those platforms. I guess maybe the Embedded group could do with having some sub categories and maybe some descriptions explaining what those categories are intended to represent?

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 9 years ago in reply to rachaelp

    Rachael,

     

    Thanks for the comment. The term definitely encompasses several sub-categories. I think we need to explain it better.

     

    Randall

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to rscasny

    I'm a fan of a good explanation and few if no subgroups.

    I have two reasons image for that:

    - subgroups create more confusion than solution.

    - blogs in subgroups don't get views, and comments are mostly from the in-crowd.

     

    That's all. I'll get my coat image

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to rscasny

    I'm a fan of a good explanation and few if no subgroups.

    I have two reasons image for that:

    - subgroups create more confusion than solution.

    - blogs in subgroups don't get views, and comments are mostly from the in-crowd.

     

    That's all. I'll get my coat image

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
Children
  • rscasny
    rscasny over 9 years ago in reply to Jan Cumps

    Short and Sweet!. Thanks.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 9 years ago in reply to Jan Cumps

    I do tend to agree, sub categories can cause confusion if there are too many and they are not well thought out and explained. If we can sort things with just better information and descriptions relating to the main group that would be fine but maybe because "Embedded" encompasses such a wide range of topics and disciplines then maybe this isn't practical and a small number of sub groups might be necessary.

     

    Best Regards,


    Rachael

    • Cancel
    • Vote Up +3 Vote Down