Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Trouble shifting 5V clock down to 3.3V
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 504 subscribers
  • Views 1616 views
  • Users 0 members are here
Related

Trouble shifting 5V clock down to 3.3V

e14 Contributor
e14 Contributor over 10 years ago

Hi Folks.

 

I have a pwm generated clock from my mcu which is at 5V. I want to step this down to 3.3V. I am using a 2N7000 N channel mosfet and the setup shown below.

 

image

 

This is the square wave generated by the mcu:

image

 

When I put it through the level shifter I get This output:

image

 

It is clearly offset and very distorted. When I apply 5V directly I get 3.3V out and when I connect ground to it I get 0V out as expected. However when I apply the 0 to 5V square wave it doesn't work.

 

Does anybody know why this is happening?

 

Thanks,

 

Mark.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 10 years ago +1
    Do it like this: R1 should be chosen according to frequency - for 50kHz 1k will be acceptable. R2 will not be necessary with a 2n7000 (apply input directly to gate.) This type of level shifter is not very…
  • Jan Cumps
    Jan Cumps over 10 years ago +1
    Mark, I've made a few videos on this subject. Having an ugly deformed signal with a voltage divider solution is normal. www.youtube.com/watch www.youtube.com/watch
  • shabaz
    shabaz over 10 years ago in reply to e14 Contributor +1
    Bit of a large package(20-pin DIP but SN74LVC244AN SN74LVC244AN is a nice part to have around It is 5V tolerant so good for level conversion particularly if you have many signals
Parents
  • DAB
    DAB over 10 years ago

    Easy answer is to use a $4 USD PSOC4 board and program a pin to output the 3.3v signal.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • DAB
    DAB over 10 years ago

    Easy answer is to use a $4 USD PSOC4 board and program a pin to output the 3.3v signal.

     

    DAB