Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum I2c peripheral library for PIC24 and example code for I2C for PIC24
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 503 subscribers
  • Views 2411 views
  • Users 0 members are here
  • i2c
  • pic24 i2c
Related

I2c peripheral library for PIC24 and example code for I2C for PIC24

vchop003
vchop003 over 8 years ago

Hello,

I am working on PIC24 and Would like to have the I@C example code for PIC24 and I2C peripheral library for PIC24.

Please suggest some documents and code. Thank you in advance!!

  • Sign in to reply
  • Cancel

Top Replies

  • genebren
    genebren over 8 years ago +3
    Greetings, I did a really quick google search and came up with the following hits: https://www.microchip.com/forums/m745734.aspx I2C Library https://engineering.purdue.edu/ece477/Archive/2009/Spring/S09…
  • 14rhb
    14rhb over 8 years ago +1
    Hi Vishal, Which toolchain are you using for development? If you are using MPLAB X or MPLAB Xpress IDE (the cloud based version) then you can use an add in tool called Microchip Code Configurator (MCC…
Parents
  • 14rhb
    14rhb over 8 years ago

    Hi Vishal,

     

    Which toolchain are you using for development?

     

    If you are using MPLAB X or MPLAB Xpress IDE (the cloud based version) then you can use an add in tool called Microchip Code Configurator (MCC) to make things a bit easier. In MCC you select the peripherals you want to work with using an intuitive GUI - then you click generate code and all the skeleton code is generated for you. You then just have to utilise it i.e. call the function to send a byte out, poll the interrupts for a I2C byte received.

     

    The nice thing about MCC is that it draws to your attention all those register flags that are required to get something working. If you work directly from the datasheet you can sometimes omit to set a single bit and .....nothing happens !

     

    regards,

     

    Rod

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • 14rhb
    14rhb over 8 years ago

    Hi Vishal,

     

    Which toolchain are you using for development?

     

    If you are using MPLAB X or MPLAB Xpress IDE (the cloud based version) then you can use an add in tool called Microchip Code Configurator (MCC) to make things a bit easier. In MCC you select the peripherals you want to work with using an intuitive GUI - then you click generate code and all the skeleton code is generated for you. You then just have to utilise it i.e. call the function to send a byte out, poll the interrupts for a I2C byte received.

     

    The nice thing about MCC is that it draws to your attention all those register flags that are required to get something working. If you work directly from the datasheet you can sometimes omit to set a single bit and .....nothing happens !

     

    regards,

     

    Rod