Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum control stepper motor with microcontroller
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 505 subscribers
  • Views 1133 views
  • Users 0 members are here
Related

control stepper motor with microcontroller

meenusaini
meenusaini over 8 years ago

hello everyone

i have to draw circle pattern with two stepper motor with microcontroller. can anybody have any idea..

 

 

thank you

  • Sign in to reply
  • Cancel

Top Replies

  • DAB
    DAB over 8 years ago +10
    Build an X-Y stage with a stepper motor driving each axis. Put a pen suspended above the center with a solenoid for up or down movement. Put a piece of paper on the X-Y stage. Set up your MCU to drive…
  • 14rhb
    14rhb over 8 years ago +8
    Hi Meenakshi, I'm sure someone on E14 will be an expert at steppers and microcontrollers, however, a little more detail from you will help get those answers quickly... Tell us a little bit about why you…
  • genebren
    genebren over 8 years ago +6
    There are many ways to do this. DAB has offered some great suggestions. To offer a little more help, depending on how much engineering your project requires and the depth of your skill set, I could offer…
Parents
  • DAB
    DAB over 8 years ago

    Build an X-Y stage with a stepper motor driving each axis.

    Put a pen suspended above the center with a solenoid for up or down movement.

    Put a piece of paper on the X-Y stage.

    Set up your MCU to drive the stage using g-code.

    Use Open SCAD to create you g-code.

    Load g-code into the MCU.

    Execute the g-code.

     

    Circle drawn.

     

    DAB

    • Cancel
    • Vote Up +10 Vote Down
    • Sign in to reply
    • Cancel
  • Fred27
    Fred27 over 8 years ago in reply to DAB

    @DAB You shouldn't need g-code - just some trigonometry and knowledge of on in-built timers on your microcontroller. Of course - this is if you will only ever want to do circles.

     

     

    There is of course the question as to why the OP want to draw circles using a microcontroller and stepper motor in the first place.

    • If you just need to draw circles, then there are certainly easier and better ways - for instance, a geared motor and a pen on an arm
    • If it's because this is a student assignment, then I'd suggest you start from your coursework and ask if you're stuck on something specific.
    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Fred27
    Fred27 over 8 years ago in reply to DAB

    @DAB You shouldn't need g-code - just some trigonometry and knowledge of on in-built timers on your microcontroller. Of course - this is if you will only ever want to do circles.

     

     

    There is of course the question as to why the OP want to draw circles using a microcontroller and stepper motor in the first place.

    • If you just need to draw circles, then there are certainly easier and better ways - for instance, a geared motor and a pen on an arm
    • If it's because this is a student assignment, then I'd suggest you start from your coursework and ask if you're stuck on something specific.
    • Cancel
    • Vote Up +3 Vote Down