Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum BLDC Motor
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 503 subscribers
  • Views 566 views
  • Users 0 members are here
  • bldc motor
Related

BLDC Motor

sekshir
sekshir over 8 years ago

I would like to develope BLDC motor driver with the help of UC 3625q. Is this IC is already preloaded the program for its itended function for driving the motor. Then I will design the circuit as per the requirements.

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui over 8 years ago +3
    It seems that the UC3625 (based on the datasheet http://pdf.datasheetz.com/data/Integrated%20Circuits%20(ICs)/Motor%20and%20Fan%20Controllers,%20Drivers/296-11235-5-data… ) seems to be designed with motor…
  • sekshir
    sekshir over 8 years ago in reply to Gough Lui +1
    Thank you for your great advice,I would certainly follow it for development.
  • Gough Lui
    Gough Lui over 8 years ago

    It seems that the UC3625 (based on the datasheet http://pdf.datasheetz.com/data/Integrated%20Circuits%20(ICs)/Motor%20and%20Fan%20Controllers,%20Drivers/296-11235-5-data… ) seems to be designed with motor control based on hall sensor feedback. The truth table is given as Table 2. Based on the application in Figure 14, it seems that there is no programming necessary, this is a fixed function IC with a number of inputs which can be used to change its operational mode. Likewise, the pin-out doesn't show any particular dedicated programming pins, so I suspect it can't be programmed like a microcontroller, instead it is "programmed" through the use of external components (e.g. resistors).

     

    - Gough

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • sekshir
    sekshir over 8 years ago in reply to Gough Lui

    Thank you for your great advice,I would certainly follow it for development.