Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum MSP430F479: The UART received data is not correct
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 503 subscribers
  • Views 379 views
  • Users 0 members are here
  • ti msp430
  • uart
Related

MSP430F479: The UART received data is not correct

sadique
sadique over 7 years ago

Hi,

I am facing a little problem with the bluetooth communication with my MSP430F479. I am using the BM70 ble module. I am trying to send two words over the transmit pin and as the buffer can only contain one byte, I am sending the Upper byte first and then the lower byte by swapping. The received first byte in the mobile app (to see the bluetooth transmitted data) is always correct that is as sent by the TX pin (using a breakpoint after each transmit to check the received byte). But for the second byte and third byte data transmitted, I am not getting the right data (it is showing wrong byte of data in the app) . The UART baud rate of the MSP430 is set 115200 Hz as the default baud rate of the BM70 ble module is also the same. I am attaching the code simulated in the IAR embedded workbench below:

#include <msp430.h>

;-------------------------------------------------------------------------------

ORG 01100h ; Program Start

;-----------------------------------------------------------------------------

RESET mov.w #0A00h,SP ; Initialize stackpointer

StopWDT mov.w #WDTPW+WDTHOLD,&WDTCTL ; Stop WDT

SetupFLL bis.b #XCAP11PF,&FLL_CTL0 ; Configure load caps

SetupP1 bis.b #03h,&P1DIR ; P1.1 and P1.2 output (LD1 output set to make the BM70 in application mode)

bis.b #03h,&P1OUT

OFIFGcheck bic.b #OFIFG,&IFG1 ; Clear OFIFG

mov.w #047FFh,R15 ; Wait for OFIFG to set again if

OFIFGwait dec.w R15 ; not stable yet

jnz OFIFGwait

bit.b #OFIFG,&IFG1 ; Has it set again?

jnz OFIFGcheck ; If so, wait some more

SetupP2 bis.b #BIT4+BIT5,&P2SEL ; P2.4,5 USCI option select

SetupUART

bis.b #UCSSEL_2,&UCA0CTL1 ; SMCLK

mov.b #09,&UCA0BR0 ; 1MHz 115200

mov.b #00,&UCA0BR1 ; 1MHz 115200

mov.b #02,&UCA0MCTL ; Modulation

bic.b #UCSWRST,&UCA0CTL1 ; **Initialize USCI state machine**

bis.b #UCA0RXIE,&IE2 ; Enable USCI_A0 RX interrupt

Mainloop mov.w #0F349h,R7 ;data to be sent

mov.w #1234h,R6 ;data to be sent

TZ1 bit.b #UCA0TXIFG,&IFG2 ; USCI_A0 TX buffer ready?

jz TZ1 ; Jump if TX buffer not ready

swpb R7 ;swapping the bytes

mov.b R7, &UCA0TXBUF ;send most significant byte

swpb R6 ; Prepare to send High Byte of Sum

TZ2 bit.b #UCA0TXIFG,&IFG2 ; USCI_A0 TX buffer ready?

jz TZ2 ; Jump if TX buffer not ready

mov.b R6, &UCA0TXBUF ; Send High Byte of Sum

swpb R6

TZ3 bit.b #UCA0TXIFG,&IFG2 ; USCI_A0 TX buffer ready?

jz TZ3 ; Jump if TX buffer not ready

swpb R6

mov.b R6, &UCA0TXBUF ; Send Low Byte of sum

LEND bis.b #LPM3+GIE,SR ; Enter LPM3, interrupts enabled

nop

;------------------------------------------------------------------------------

USCIA0RX_ISR; Echo back RXed character, confirm TX buffer is ready first

;------------------------------------------------------------------------------

TX0 bit.b #UCA0TXIFG,&IFG2 ; USCI_A0 TX buffer ready?

jz TX0 ; Jump if TX buffer not ready

;mov.b &UCA0RXBUF,&UCA0TXBUF ; TX -> RXed character

bic.w #LPM3,0(SP) ; Turn the CPU back on

reti ;

;

;------------------------------------------------------------------------------

; Interrupt Vectors

;------------------------------------------------------------------------------

ORG 0FFFEh ; RESET Vector

DW RESET ;

ORG 0FFF2h ; USCI_A0 Rx Vector

DW USCIA0RX_ISR ;

END

  • Sign in to reply
  • Cancel
  • rsjsouza
    rsjsouza over 7 years ago

    I don't have IAR nor the same device, but there is are several assembly example projects in the TI Resource Explorer

     

    An assembly implementation of a 115200bps full duplex UART and using USCIA0 is available at this link (there are others).

     

    Hopefully this helps you figure out the exact conditions for your project.