Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum PIC32 delay help
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 505 subscribers
  • Views 2843 views
  • Users 0 members are here
  • programming.
  • timer
  • delay_timers
  • pic32
Related

PIC32 delay help

sanyika95
sanyika95 over 7 years ago

Hello everyone!

 

I just started to learn PIC32 programming with a PIC32 Ethernet Starter kit. I wanted to blink its led, 1 second on - 1 second off.

 

Here is the code for the delay:

#define USHORT unsigned short

void delayMs(USHORT milisec) {
    T1CON = 0x8010;
    TMR1 = 0x00;
    USHORT i = 0;
    PR1 = 0x40;
    while(i != milisec) {
        while(TMR1) {
        }
        i++;
        TMR1 = 0x00;
    }
    T1CON = 0x00;
    return;
}

 

It just works (or it looks like to work, I haven't measured it with an oscilloscope, just with a "stopwatch") and I don't know why. Can someone explain me?

 

 

The datasheet of the kit:

http://ww1.microchip.com/downloads/en/DeviceDoc/61166A.pdf

 

The datasheet of its PIC:

http://ww1.microchip.com/downloads/en/devicedoc/60001156j.pdf

  • Sign in to reply
  • Cancel

Top Replies

  • fmilburn
    fmilburn over 7 years ago +2
    I am not familiar with the PIC32 but that is strange code. You need to know what the clock speed is and how the dividers to the timer are set. A quick look at the datasheet shows that T1CON is the timer…
  • sanyika95
    sanyika95 over 7 years ago in reply to fmilburn +2
    I don't really know the clock speed. In the datasheets there were a 32kHz and a 8MHz clock as internal. I did my calculation with both of them and none of them worked. As you said, the T1CON is the control…
  • rusgray
    rusgray over 7 years ago +2
    Have you done the simple beginner Harmony tutorial project ? It implements a blinking LED, and does a good job of covering the basics of working with Harmony. It also serves as a good starting point for…
Parents
  • divya1213
    divya1213 over 7 years ago

    As I am getting you right, You said TMR1 is incrementing once per millisecond, but the TMR1 register will increase at every hit of the clock! So it has to reach X bit, depending on the clock and the prescale to wait 1 millisecond. The PR1 is the value when to reset the TMR1.

    Here if you want to start your Embedded Training in Noida then join them.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • divya1213
    divya1213 over 7 years ago

    As I am getting you right, You said TMR1 is incrementing once per millisecond, but the TMR1 register will increase at every hit of the clock! So it has to reach X bit, depending on the clock and the prescale to wait 1 millisecond. The PR1 is the value when to reset the TMR1.

    Here if you want to start your Embedded Training in Noida then join them.