Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Get Your Xilinx FPGA/Programmable SoC Questions Answered here
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 40 replies
  • Subscribers 512 subscribers
  • Views 6990 views
  • Users 0 members are here
  • soc
  • answer
  • xilinx
  • fpga
  • questions
Related

Get Your Xilinx FPGA/Programmable SoC Questions Answered here

rscasny
rscasny over 7 years ago

In the past year or so, the element14 community has been offering quite a few programs, contests, and initatives around Xilinx's FPGA and heterogeneous SoC, ZYNQ. We have hosted webinars, run roadtests, and offered a training program last year called Path to Programmable.

 

I see element14 member interest in Xilinx product knowledge on the rise. I plan on offering more Xilinx-related projects and roadtests in the coming months. (Stay tuned to Path to Programmable 2 with the Ultra96v2) Given all this activity, I thought it would be a great idea to bring in a Xilinx product expert for some well needed Q&A time. So let me introduce you to Adam Taylor ( adamtaylorcengfiet ).

 

I believe Adam has been an element14 member for several years. He is the Director of ADIUVO Engineering. He is a Chartered Engineer and Fellow of the Institute of Engineering and Technology. He is well known for his Microzed Chronicles. He writes the Exploring the Programmable World for element14. Adam has been instrumental in developing element14's FPGA/Programmable SoC Essentials.

 

Adam also is an expert in the PYNQ framework: Python for ZYNQ productivity. So, if you are asoftware developer who wants to explore the Programmable world, I'd encourage you to ask Adam your top questions.

 

So, if you have any questions revolving around FPGAs, programmable SoCs, a project in progress, perhaps even a question about Vivado, please click REPLY and asked them here.

 

Sincerely,

 

Randall Scasny

-element14 Team

  • Sign in to reply
  • Cancel

Top Replies

  • jomoenginer
    jomoenginer over 7 years ago +4
    Awesome! It's great that adamtaylorcengfiet is a resource on element14 for Programmable SoC questions. I'm sure I will have many as I finish my Digilent Zybo Z7 RoadTest. I do find Adam's Microzed Chronicles…
  • jomoenginer
    jomoenginer over 7 years ago +4
    For what it's worth, there is an Integrating Arm Cortex-M soft CPU IP into FPGAs virtual workshop that features Adam Taylor as an instructor and uses the Digilent Arty S7-50T to be held August 14th, 2019…
  • wolfgangfriedrich
    wolfgangfriedrich over 7 years ago +3
    I would appreciate any comments on a process on how to make the DDR3 SDRAM MIG work without using the AXI interface in VHDL. As a target platform I have the Digilent Arty S7 board. I tried this during…
Parents
  • neuromodulator
    neuromodulator over 7 years ago

    - What trends do you see happening in the FPGA world in the upcoming years?

     

    - Do you see FPGAs moving into the realm of PC's? GPUs, even though they are completely different, have gained a lot of attention in the general computation arena, while at the same time FPGAs haven't apparently gained much more popularity. What do think is the cause of this?

     

    - Do you see any upcoming official opening of the bitstream formats? The formats appear to be slowly being reverse-engineered, whats is the rationale in keeping them closed? I would think that opening them would allow the creation of an ecosystem of 3rd party tools which probably would attract more users to the platform. Making software opensource could also lower development costs, etc. What are your thoughts on all this?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • adamtaylorcengfiet
    adamtaylorcengfiet over 7 years ago in reply to neuromodulator

    These are great questions.

     

    I think the trend is pretty clear they are evolving (and have been for many years) in to platforms, which combine different compute engines e.g Programmable Logic and Processors cores. The Xilinx Versal devices take this to the next step. These heterogeneous devices enable the deployment of elements of the application being developed to the most optimal compute engine, what we will see along with rapid device development in this area is a significant increases in development SW which offers a combined platform which can be used to develop the application and then deploy elements as required in the different engines example include SDSoC, SDAccel for example.

     

    I am not sure PC's will ever contain a programmable logic device on board the motherboard but I think programmable logic will be easily available via the cloud e.g. AWS and using modules like the Alveo card either locally or in the cloud. GPU's became popular for computation as PC do need them as well for graphics in a number of applications therefore it was a natural extension to be able to use them for computation as needed.

     

    I do not and I am not sure why people get hung up on it in my opinion. I am not 100% sure why they are kept closed behind the need for IP protection and most importantly getting the bitstream wrong could potentially damage the device which will cause several issues. If it was me I would focus open tool development on areas such as simulation, verification, synthesis, formal verification etc I know there is work going on in this area. Regarding development costs, most vendors offer free versions which cover a significant range of components, which should address the most maker, hobbyist and many commercial applications. While the larger projects using tools which require licensing are often developed by organisations which can afford the costs. I have also found the vendors very willing to talk and support if your doing interesting projects.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jomoenginer
    jomoenginer over 7 years ago in reply to adamtaylorcengfiet

    adamtaylorcengfiet  wrote:

     

     

    I am not sure PC's will ever contain a programmable logic device on board the motherboard but I think programmable logic will be easily available via the cloud e.g. AWS and using modules like the Alveo card either locally or in the cloud. GPU's became popular for computation as PC do need them as well for graphics in a number of applications therefore it was a natural extension to be able to use them for computation as needed.

     

     

    Actually, FPGAs have been placed on Motherboards for some time now,.

    https://www.anandtech.com/show/11960/asus-announces-ws-c621e-sage-workstation-motherboard-dual-xeon-overclocking

     

    Intel is now producing Xeon processors that include a FPGA in the same package as well as offering the Intel Acceleration Stack for Intel XeonRegistered CPU with FPGAs.  However, as you mentioned, these would be more inline with the Web Giants and such due to the cost of the devices at this time. 

     

    I like the comment regarding open source tools.  This is starting to be a thing now where folks are getting frustrated with the FPGA vendor tools and are reverse engineering the FPGA code to create their own open source tools to program the device. I suspect this will continue to expand.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • adamtaylorcengfiet
    adamtaylorcengfiet over 7 years ago in reply to jomoenginer

    I knew FPGA where on motherboards but as I understand it, it is not accessible by the user for programming instead it is smallish device which provides functions on the motherboard design. I read the question as being will FPGA be deployed on motherboards in a manner that they are accessible by the user to program and accelerate algorithms like you can with GPU's

     

    It will be interesting to see what the open source community does, I suspect your right re reverse engineering.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • adamtaylorcengfiet
    adamtaylorcengfiet over 7 years ago in reply to jomoenginer

    I knew FPGA where on motherboards but as I understand it, it is not accessible by the user for programming instead it is smallish device which provides functions on the motherboard design. I read the question as being will FPGA be deployed on motherboards in a manner that they are accessible by the user to program and accelerate algorithms like you can with GPU's

     

    It will be interesting to see what the open source community does, I suspect your right re reverse engineering.