Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Pic Microcontrollers Forum Programming a real randomize timer
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 237 subscribers
  • Views 894 views
  • Users 0 members are here
Related

Programming a real randomize timer

e14 Contributor
e14 Contributor over 15 years ago

Hello together.

 

I would like to write a program that give me a random number (range: no matter). I can't realize it. I use PIC controllers, may that could help you to give me an answer. Program languages are C or BASIC.

 

Please help me. Thank a lot!!

  • Sign in to reply
  • Cancel
Parents
  • Jorge_Garcia
    Jorge_Garcia over 15 years ago

    Hi Christian,

     

    I hope you are doing well. It's important to realize that computers can't generate true random numbers, because they are deterministic. Every piece of code you will ever find for random number generation will generate a Pseudo Random Number, within a limited range the probability distribution will be approximately flat approximating randomness.

     

    With that said just use the rand() function included with C.

     

    At the top of your code

     

    #include <stdlib.h>

     

    This will include the standard library header which includes the rand() function. I can't help you much more than that because my PIC programming is a little rusty and I don't want to mess you up. This should take care of your problem.

     

    Also you'll have to seed this function if you want to get a different series of random numbers every time you run the application. If you google the library or the rand() function you should find what you need.

     

    hth,

    Jorge Garcia

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to Jorge_Garcia

    I was feared that I get this answer!

     

    But i have the idea to solve the problem with a hardware solution.

     

     

    I'll connect a capacitor to an analog input, load it, stop loading, unload it (with resistor), wait a few ms, and read in the voltage. May the discharge level is irregular enough to get a random number?!

     

    What do you think?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jorge_Garcia
    Jorge_Garcia over 15 years ago in reply to e14 Contributor

    Hi Christian,

     

    I agree that the only way to get a true random number is with an analog solution. The RC circuit idea however will not work. RC discharge follows an exponential function which is very predictable.

     

    The implementations of random value generators I've seen used diodes. Try googling random number generation, you should be able to find some information on using diodes to generate random numbers. Be warned these devices are not easy to make, because the random component is a very low-level signal and you'll have to do some processing in order to get a useable value.

     

    hth,

     

    Jorge Garcia

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Jorge_Garcia
    Jorge_Garcia over 15 years ago in reply to e14 Contributor

    Hi Christian,

     

    I agree that the only way to get a true random number is with an analog solution. The RC circuit idea however will not work. RC discharge follows an exponential function which is very predictable.

     

    The implementations of random value generators I've seen used diodes. Try googling random number generation, you should be able to find some information on using diodes to generate random numbers. Be warned these devices are not easy to make, because the random component is a very low-level signal and you'll have to do some processing in order to get a useable value.

     

    hth,

     

    Jorge Garcia