Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Pic Microcontrollers Forum Trying to identify the purpose of a circuit with a PIC18LF6622
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 1 answer
  • Subscribers 238 subscribers
  • Views 2205 views
  • Users 0 members are here
Related

Trying to identify the purpose of a circuit with a PIC18LF6622

ghstridr
ghstridr over 9 years ago

image

 

 

image

I'm wondering if anyone can help me in identifying the purpose of this board?

I found it walking to my car in parking garage. It was packaged professionally in a project box with 2xAA for power (3V) and some silica gel.

The lid has a rubber gasket embedded. No openings or access through the box or lead without opening it up. No markings on the outside or inside other than what is silk screened on the board.

I think that is a 5 pin jtag type port on the left side of the board. The two silvered components are rf transceivers, large one operates 433.72mhz to 434.12mhz and the small one on the left is 916.3mhz to 916.7mhz. Pulled that data from Mouser.

Thanks!

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 9 years ago in reply to ghstridr +3 suggested
    Hi Michael, That gets more interesting.. I could just about read the marking on U1, but not U2. However, the marking of U1 is HMC52L which is more than likely a Honeywell HMC1052L (PDF Datasheet) device…
  • ghstridr
    ghstridr over 9 years ago in reply to shabaz +2
    That sounds very plausible. The garage does have signage to indicate whether the garage is full or not. This must have been some where above one of the ramps or the entrances/exits.
  • rachaelp
    rachaelp over 9 years ago +1
    Well you say you found it as you were walking to a car parking garage? Clancy Systems do parking citation equipment. Could it be the main board for one of these parking ticket printers? http://www.clancysystems…
Parents
  • mcb1
    0 mcb1 over 9 years ago

    Using Google shows Clancy Systems are involved with Parking (usually enforcement).

     

    I suspect it is some form of access control board.

    Possibly the receiver for remote control but linked to a database or internal stored.

    It may be a repeater using the two different frequencies.

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 9 years ago

    Using Google shows Clancy Systems are involved with Parking (usually enforcement).

     

    I suspect it is some form of access control board.

    Possibly the receiver for remote control but linked to a database or internal stored.

    It may be a repeater using the two different frequencies.

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • ghstridr
    0 ghstridr over 9 years ago in reply to mcb1

    I called them and left a message with their tech support on the off chance it is a piece of their equipment.